STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FDCAN - No buffer space available

I'm trying to run STM32MP1 with two CAN FD drivers connected to PD0/1 and PB5/13.I have connected saleae analyzer to all four TX, RX lines and there is no changes during candsend command. I got only " write: No buffer space available" message.How to ...

tj5 by Associate
  • 3365 Views
  • 3 replies
  • 0 kudos

Hai , We want to use STM32MP15x series device in our projects, for this device we need supported IDE for the A7 core accessing and for compiling the source .Like M4

For STM32MP1 device we can able to check the M4 device in keil 5 . We are un able to get the cortex A7 device . Can you please suggest the supported IDe for A7. We don't want to use the os We want to use freeRtos.

srikanth by Associate III
  • 1572 Views
  • 2 replies
  • 0 kudos

bitbake uboot error , pls help

NOTE: Executing SetScene TasksNOTE: Executing RunQueue TasksERROR: u-boot-stm32mp-extlinux-2.0-r0 do_create_multiextlinux_config: Error executing a python function in exec_python_func() autogenerated:The stack trace of python calls that resulted in t...

Ara.1 by Senior
  • 2140 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.