STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! qt5 stm32mp135

Hi,I encounter a performance issue on the qt5 application on STM32MP135. I build a simple application with three plaintextedit objects showing temperature with 1s period from ds18b20. Everything compiles well and works, but the refreshing temperature...

MWoło.2 by Senior III
  • 4601 Views
  • 5 replies
  • 0 kudos

Why does STM32MP1 DMA ADC work in Engineering mode, but not in when I compile it and use `fw_cortex_m4.sh`?

First I declare the buffer length/* USER CODE BEGIN PD */ #define ADC_BUF_LEN 10000Then I declare the buffer/* USER CODE BEGIN PV */ GPIO_InitTypeDef gpio_init_structure; VIRT_UART_HandleTypeDef huart0; VIRT_UART_HandleTypeDef huart1; uint16_t a...

msche.1 by Associate III
  • 3787 Views
  • 5 replies
  • 1 kudos

Uboot Environment Configuration

Hello, i am using an stm32mp1-dk2 board. For using fw_printenv and other uboot tools from user space one must define a "/etc/fw_env.config" file. I can see that the "/uboot.env" file is driectly saved under the root "/" and so i defined the "fw_env.c...

ajava by Associate II
  • 9223 Views
  • 9 replies
  • 0 kudos

STM32MP1xx DNS Openstlinux

Hi,my question is how to set up resolv.conf with the DNS nameserver not to lose it after reboot.Some of the manuals on the internet want to modify /etc/systemd/resolved.conf by uncomment DNS line and provide a valid ip. Unfortunately, it's not workin...

MWoło.2 by Senior III
  • 1161 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.