STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Wakeup from shutdown using RTC

Hello everyone,I am working on a custom board based on stm32mp15x. I am trying to periodically wake up my system from the shutdown condition using the RTC. From the hardware point of view, I am using the STPMIC to restore the Vdd supply of the MPU, w...

bimorqt by Associate III
  • 4081 Views
  • 1 replies
  • 0 kudos

Problem with controlling GPIO

Hi.I have a problem with controlling the LED on the stm32mp135f-dk board.bashroot@techs:~# gpioinfo -c0gpiochip0 - 16 lines: line   0: "PA0"            input line   1: "PA1"            input consumer="kernel" line   2: "PA2"            input consumer...

"panel-simple.c" customization errors

This post is connected to my previous one "Display customization". I created this new post because I can't insert replies in the previous one "Display customization"I created the following patch to modify the panel-simple.c file diff --git a/drivers/...

nataut by Associate III
  • 1538 Views
  • 0 replies
  • 0 kudos

Display customization

Hi All,In my currently yocto image I want to customize a LCD TFT RGB 7" 1024x600 24bpp display. At the moment, I have a dts patch file where there are all image customizations. In this file the currently display settings (LCD TFT RGB 7" 800x480) are ...

nataut by Associate III
  • 8132 Views
  • 8 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.