2023-07-19 1:20 AM
Hello, I have an interprocessor communication problem using the OpenAMP_TTY_echo example on the STM32MP157C-EV1 board.
I am tring example OpenAMP_TTY_echo, to comunicate between M4 and A7 on the STM32MP157C-EV1 board.
I can't find the solution, and I need your help.
I installed Linux (en.flash-stm32mp1-openstlinux-6-1-yocto-mickledore-mp1-v23-06-21.tar.gz) downloaded from:
https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-EV1/Let%27s_start/Populate_the_target_and_boot_the_image
and installed to the STM32MP157-EV1 with STM32 Cube Programmer V2.14.0
On my PC: I am using Keil V5.36, compiled the example OpenAMP_TTY_echo without error.
The example code runs without problem. either with the Tools: STM32MP1 Load and Run command, or from the Debugger.
I traced the code and it runs normally in the while(1) loop of app_main (main.c)
(without going through an "Error_Handler")
When I execute ssh command to connect to the STM32MP157-EV1 board, it seems that none of the devices ttyRPMSG0 or ttyRPMSG1 are present.
ls /dev/ttyRPMSG*
ls: cannot access '/dev/ttyRPMSG*': No such file or directory
So no communication (echo) between the A7 and the M4 as indicated in the doc:
Using STM32MP1 Cortex-M with Keil MDK, MDK Tutorial, AN319, February 2021, V1.2
stty -onlcr -echo -F /dev/ttyRPMSG0
stty: /dev/ttyRPMSG0: No such file or directory
Do I need to do anything special on the linux side? Am I doing something wrong?
Thank you for your help.
Pierre-Alain
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.