STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Dual Ethernet and Fiber with Stm32 MPU?

Hi dear all,I'm looking for dual ethernet examples to implement with my stm32mp157d MPU , but I couldn't find anything on the internet.I've seen that there is no STM32 with dual ethernet interface but i want to add dual ethernet and fiber ports to my...

Zaim by Associate II
  • 3468 Views
  • 2 replies
  • 0 kudos

Ethernet not working in u-boot: "Could not get PHY for ethernet@5800a000: addr 0 phy_connect() failed"

hi,I am working with a custom board based on the STM32MP157C. I use a lan9303 chip which is acting as a switch for ethernet. In the linux kernel, there are no problems with the ethernet but I can't get it to work in u-boot. Even when I use the same D...

sgtl5000 codec dsi i2c

Hi All,i am using stm32mp1 with i2c on sgtl5000 codec and control lines are over carrier i2si am getting kernel soc sgtl5000.c error sgtl5000 0-000a: Error reading chip id -6<STM32_PINMUX('A', 15, AF5)>; /* I2S1_WS */<STM32_PINMUX('Z', 0, AF5)>, /* I...

Ara.1 by Senior
  • 18822 Views
  • 52 replies
  • 0 kudos

Resolved! Uboot not executing board_init function?

I'm using the bootlin buildroot branch: st/2021.02.I want to run a certain function on init of the Uboot (board_init function), like the ones used for the DK1 and DK2. My problem is that the function doesn't seem to be called. I have tried to debug t...

jhi by Senior
  • 1900 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.