STM32 MCUs
From FAQs to complete How-to articles, find useful articles on STM32 MCUs programming, troubleshooting, ecosystem, and product details.
cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge base articles

How to install X-CUBE-AI through STM32CubeMX

This installation guide shows how to install the X-CUBE-AI expansion package through STM32CubeMX.  X-CUBE-AI is an STM32Cube expansion package that expands the capabilities of STM32CubeMX and is a part of the STM32Cube.AI ecosystem. It offers automat...

AMEMCUSupportCenterAD_0-1693955140456.png AMEMCUSupportCenterAD_1-1693951057612.png AMEMCUSupportCenterAD_4-1693960172543.png AMEMCUSupportCenterAD_5-1693960208871.png

How is my SPI's baudrate calculated using STM32CubeMX?

STM32CubeMX is a graphical tool that allows users to configure STM32 MCUs (microcontrollers) and MPUs (microprocessors) quickly and simply. In addition, the tool also assists in generating the corresponding initialization C code for the Arm Cortex-M...

StefanieLAU_1-1693987620071.png StefanieLAU_2-1693987620069.png StefanieLAU_3-1693987620073.png StefanieLAU_4-1693987620075.png

How can I output a clock signal to the STM32’s MCO pin?

STM32CubeMX is a graphical tool that allows users to configure STM32 MCUs (microcontrollers) and MPUs (microprocessors) quickly and simply. In addition, the tool also assists in generating the corresponding initialization C code for the Arm Cortex-M...

StefanieLAU_0-1693989229209.png StefanieLAU_1-1693989229188.png StefanieLAU_2-1693989229191.png StefanieLAU_3-1693989229204.png

Custom external loader "failed to download segment[0]"

Why do I get an "failed to download Segment[0]" error when using a custom external loader in STM32CubeProgrammer version 2.7.0 or higher? The trace shown below is only an example, some values may vary, but the main point is that an error is raised (a...

How does the ThreadX Semaphore work

ThreadX provides 32-bit counting semaphores that range in value between 0 and 4,294,967,295. There are two operations for counting semaphores: tx_semaphore_get and tx_semaphore_put. The get operation decreases the semaphore by one. If the semaphore i...

249.gif 250.png 251.png 252.png

How to reach 480MHz for STM32H7xx MCUs

You can reach 480MHz only for the following STM32H7 part numbers:  STM32H747/757 STM32H745/755 STM32H743/753STM32H742STM32H750 Note: For some parts, you need to check the maximum frequency from the datasheet.This is not enough! you also need to check...

1672.png 1673.png 1674.png 1675.png
Foued_KH by ST Employee
  • 6919 Views
  • 0 comments
  • 5 kudos

How to connect a J-Link debug probe to the Nucleo-WB55RG

1. Introduction Onboard, the NUCLEO-WB55RG includes a ST-LINK/V2-1 debugger/programmer with USB reenumeration capability: mass storage, virtual COM port and debug port.The ST-LINK/V2 is an in-circuit debugger and programmer for the STM8 and STM32 mic...

1013.png 1014.png 1015.png 1016.png