2022-05-16 12:12 AM
Hi,
I am using a STM32WB55 board and its USB Dongle.
I set up a ZigBee network with Messaging Cluster between them.
The WB55 is the router + server, and the Dongle is the coordinator + client.
I can send a Message from WB to Dongle.
When I try to send data from Dongle to WB, the callback on WB is never called, even when I send the message to everyone (broadcast).
What can make a Callback never activated?
Best regards,
CD
2022-05-16 5:35 AM
Did I send data to the wrong address?
Why the broadcast hasn't made the trick?
dst.mode = ZB_APSDE_ADDRMODE_SHORT;
dst.endpoint = SW1_ENDPOINT;
dst.nwkAddr = 0xffff;I've seen this: "Before joining a Zigbee network, a device with an IEEE 802.15.4 compliant radio has a 64-bit address that is globally unique." from the datasheet.
How can I find this address?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.