NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
In STM32CubeIDE -> Middleware -> STM32_WPAN-> BLE Application and services, there are 2 parameters "Custom P2P server" and "Custom template". How are they different and under what conditions should be used?
HelloI am able to succesfully run the "RF Tests" using a nucleo board (STM32WB55) and a dongle, both connected on the same computer via virtual com port.Now I'd like to change some parameters for the test, e.g. the TX interval on the nucleo board. I ...
Reference: https://www.st.com/resource/en/application_note/an4760-quadspi-interface-on-stm32-microcontrollers-and-microprocessors--stmicroelectronics.pdfIs there a particular reason (technical or HAL-driver related) that is behind this non-inclusion ...
Hello, I am working on an application and the power consumption is a bit high as of now. I would like to know the different low power modes and how to wake up from those modes. Could you please help me with the documentation and sample codes?
We've switched to new DC-DC(LM3281) for main power supply and found that BLE TX stopped working correctly and not passing packet test anymore.After deeper investigation we found that our DC-DC in ECO mode has ripple/pulsation of 60mV/50uS, which caus...
Recently i experimented with the RTC modules and came accross an issue where HAL_RTC_Init() fails because RTC_EnterInitMode() fail with HAL_TIMEOUTAfter debugging, it seems that HAL_PWR_EnableBkUpAccess() need to be called before HAL_RTC_Init()It app...
Hi i am developing a BLE-UART bridge with an STM32WB5M.I am guetting around 1,85 KB/s data troughput, is this normal?Did anyone pull this off with greater data troughput? (same uart thing or any streaming application)
I am using STEVAL-STRKT01 with FP-ATR-LORA1. I have successfully joined the LoRa network (US915), but whenever the device tries to send data on the network it returns "Send Error" over the serial. By debugging the code, I have tracked the cause to be...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.