2020-03-18 4:23 AM
I am developing with the stm32wb nucleo kit, and I am testing the stBleSensor application, I have tried to update the Wireless Stack sending an erroneous file (pdf), and what happens is that it updates without problem and does not give any error, but the Wireless stack does not work until I program it again via cli commands, at what point is the Wireless stack deleted during the update procedure? Is nothing checked before deleting the previous one and trying to install the new one?
2020-03-18 8:58 AM
I have noticed that the Option byte SBRV value when that happens is 0x3D000 and after connecting and disconnecting from ST cube Programmer it changes to 0x32C00 and works, why is this and how could i solve it?
2020-03-19 2:50 AM
HI,
And then when i execute this command via cli --> STM32_Programmer_CLI.exe -c port=usb1 -r32 0x20030030 1 i get:
USB speed : Full Speed (12MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in FS Mode
SN : 20803176554D
FW version : 0x011a
Device ID : 0x0495
Device name : STM32WBxx
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M0+/M4
0x20030030 : 00000000
So i have to install the fus again, why is this due to?
2020-03-20 6:57 AM
Hi Remi,
this error was produced because i add in the BLE OTA example 2 Software resets( lines 306 and 354 of app_entry.c.), in order to have an application that could recover after a Wireless Stack Update automatically without any user manual reset or something...
My question now is, i know that i read FUS version 0x0000000, because and error during update process of the Wireless Stack, (the 2 resets that i add in the code), but as in the beggining of the code there is a function: SHCI_C2_FUS_GetState which after 2 calls (check page 3 in https://www.st.com/resource/en/application_note/dm00513965-st-firmware-upgrade-services-for-stm32wb-series-stmicroelectronics.pdf ) should activate FUS and recover the properly Wireless Stack behaviour, why is code execution blocked in that function?.
The only way to recover is:
Send 2 FUS_GET_STATE comands, i dit it via cli commands, conected in usb BOOT mode interface, and then check FUS version wich is correct, then after that everything is ok, i wonder why if BLE_OTA firmware sends that commands at the beginning, it doesnt recover after 2 resets... it stays blocked there.. is it due to different behave when connected in usb Boot Mode?, i did not found documentation about it.
Regards
Alvaro
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.