STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4119 Views
  • 0 replies
  • 3 kudos

Resolved! P-NUCLEO-WB55 running PWR_STANDBY_RTC example

I am trying to set a baseline for low power measurements in my own application. To do this, I imported the PWR_STANDBY_RTC example in the STM32Cube_FW_WB_V1.3.0 repository and installed it on the P-NUCLEO-WB55. I then powered the board via 5V_EXT and...

crwper by Senior
  • 1188 Views
  • 2 replies
  • 0 kudos

About TSC function of STM32WB55CGU6

Hello there! I am debugging the TSC function of the STM32WB55CGU6. I cannot set the TSC function in MubeMX. However, in the official materials, I learned that the TSC function can be supported through the txt file. Refer to the STM32L476G_EVAL board ...

cxiao.2 by Associate II
  • 1391 Views
  • 1 replies
  • 0 kudos

Resolved! ST Nucleo WB55RG - Can't enter DFU anymore

Hello,After playing around with the Nucleo board and wanting to try the simple BLE Beacon example, I believe I somehow got the bootloader stuck.I could enter DFU mode the first time and flash accordingly to the instruction given. However, trying to ...

Resolved! "Error: -- Reserved --" message when trying FUS upgrade via SWD

Hi everyone,Up until now I've been doing FUS upgrades and BLE stack flashing on my WB55 Nucleo through the USB bootloader interface, but given that my final PCB won't have a USB port on it (space restrictions), I've had to start learning how to flash...

LW.1 by Associate II
  • 2451 Views
  • 4 replies
  • 0 kudos

WB55 Nucleo always drops to Default_Handler() -> infinite loop

Hey guys,now that the problem with the linker table is finally fixes with FW1.3.0 I have encountered another problem:If I create a new project in CubeIDE using the standard pin configuration for the WB55 Nucleo board and start debugging after the ini...

PDeng by Associate II
  • 3418 Views
  • 6 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.