2024-10-17 6:23 AM
Hi,
where can i find the OTA-Bootloader for STM32WBA55?
For STM32WB it is located in the regarding FW-Package in Folder "BLE_Ota", but in the FW-Package of STM32WBA i can't find it there.
Solved! Go to Solution.
2024-10-17 6:57 AM
Hello @ledi001
For the OTA on the STM32WBA, there is no binary file such as the "BLE_OTA" on the STM32WB. The only available firmware examples for OTA on the STM32WBA are BLE_HeartRate_ota and BLE_p2pServer_ota.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-17 6:57 AM
Hello @ledi001
For the OTA on the STM32WBA, there is no binary file such as the "BLE_OTA" on the STM32WB. The only available firmware examples for OTA on the STM32WBA are BLE_HeartRate_ota and BLE_p2pServer_ota.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-24 2:55 AM
Hi,
You can find more information on how OTA works on WBA here :
STM32WBA Bluetooth® LE – Firmware update over the air - stm32mcu
BR, Joé
2024-10-26 1:53 AM
Hello @STTwo-32 ,
thanks for information.
But when i check the linker script files, i see these Memory Definitions:
BLE_p2pServer_ota
/* Memories definition */
MEMORY
{
RAM (rw) : ORIGIN = 0x20000020, LENGTH = (128K - 0x20)
NVM (r) : ORIGIN = 0x080FC000, LENGTH = 16K
DATA (r) : ORIGIN = 0x080FA000, LENGTH = 8K
FLASH (rx) : ORIGIN = 0x08006000, LENGTH = 488K
}
BLE_ApplicationInstallManager
/* Memories definition */
MEMORY
{
RAM (rw) : ORIGIN = 0x20000010, LENGTH = (0x10000 - 0x10)
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 0x6000
}In this case, so if the OTA bootloader is included here for BLE_p2pServer_ota, shouldn't the area for the flash also start at 0x0800 0000?
2024-10-26 3:46 AM
Hello @ledi001
This is a new question. Could you please close this topic by selecting the answer of your original question as best answer. Then, create a post for your New question with more details if possible.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.