STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

STM32WL55 High power TX @ 1.8V

Hi,i am working within a 1.8V system for digital supply. I am currently designing the schematic but I struggle how to integrate the STM32WL55 into an 1.8V system while assuring I am able to achieve +22dBm output power. The issue is that the datasheet...

Albi G. by Senior
  • 3458 Views
  • 4 replies
  • 0 kudos

Resolved! Wireless controller

Hello, can somebody help me to select the STM32 controller and it's developer board for my first project that involves:wireless air mouse with keyboard and TV controller?

GS2 by Senior II
  • 7974 Views
  • 24 replies
  • 3 kudos

Resolved! WB55: Can BLE_Zigbee_Static enter Stop2 mode?

Hello,I am using Nucleo-64 to evaluate the Zigbee power consumption of WB55. When testing Zigbee, it can be seen that after adding Zigbee, the power consumption of the development board is significantly reduced, and the measured average current does ...

DL_Weng by Associate II
  • 2035 Views
  • 3 replies
  • 0 kudos

Resolved! sending photo with zigbee

I take a photo with ov2640 camera. I try to send this photo with zigbee protocol from router to coordinator. I achive this but there is a problem. After I send a photo the communication is locked totally and I can't send any data.Does zigbee protocal...

Ndemir by Associate II
  • 6244 Views
  • 14 replies
  • 3 kudos

BLE extended advertising parsing

  Hello Team ST, I am currently working on parsing my extended BLE data using the BLE_p2pClient_Ext application, specifically the `analyse_ext_adv_report` function to view the advertising data. However, I am having trouble parsing and appending the f...

Hardik02 by Associate II
  • 1638 Views
  • 2 replies
  • 0 kudos

STM32WB Low Power mode

Here's a revised version of your message:---Hi,I am using the NUCLEO-WB15CC board for a custom application where I read an analog sensor value with a 12-bit ADC resolution. The issue arises when I try to transmit this data over BLE. I am using the fo...

STM32WL5Mo dosent respond to ST-LINK

Hello,I'm trying to connect my ST-LINK-PWR V3 to my own bord with a STM32WL5M0 but it doesn't wrok. I also tried with a J-Link probe and a Nucleo board and that doesn't work either.I modified my card to work at 3.3V, no improvement.The MCU is fresh f...

laesser_0-1729496289715.png
laesser by Associate II
  • 1250 Views
  • 1 replies
  • 0 kudos

STM32WB09: Cannot build BLE project

I cannot build a simple BLE project using the newest version of STM32CUBEIDE (1.16.1) for the STM32WB09KE.Steps taken:Create new project for the STM32WB09KE.Enable all dependencies needed for RADIO, RADIO_TIMER and STM32_BLE, and enabled those.When t...

s215477 by Associate II
  • 2763 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.