NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I have a self-design STM32WB board and properly flash "stm32wb5x_FUS_fw.bin", "stm32wb5x_BLE_Stack_full_fw.bin" and "BLE_TransparentMode_reference.hex" STM32_Programmer_CLI.exe. Now I am trying to use STM32CubeMonitor-RF. When I try to connect to it ...
The Mesh Library file ist in STM32CubeWB\Middlewares\ST\STM32_WPAN\ble\mesh\Library.And the user API is in ble_mesh.h.When i want to use it how it is described in ble_mesh.h there are many undefined references, so i have to implement many functions, ...
hello thereI am useing stm32L496 with SX1262DVK1DAS lora module.As firmware, I am using the latest firmeware I-CUBE-LRWAN 2.1.0As lorwan server is am useing public lorawan network.I am testing my device with CLASS_A and CLASS_C modes.my Lorawan peram...
Hi everyone!I am trying to make the LoRaWAN Fragmented Data Blok Transport package work. As a first step, my goal is to send a file such as a txt document (or whatever) to my end-device.I work with a STM32WL and an End_Node project. I have already ad...
Hi,I have stm32wle5 and a circuit to measure current. stm32 will generate a PWM using timer1 ch1. The opamp's output is also connected to the ADC input of stm32. I want to measure the current (read ADC values) when PWM is on. Preferably in the middle...
I am using the LPTIM1 to aquire a sensor measurement trough interruption each T period. When I set it in continous mode (reference manual says: To enable the continuous counting, the CNTSTRT bit must be set) everything works out well. HAL_LPTIM_TimeO...
안녕하세요 개발�?입니다.현재 Bluetooth 쪽 관련 개발�?� 하고 있습니다.문�?�드릴 내용�?� P-NUCLEO-WB55 개발보드�?�STM32WB55RGV6, STM32WB55CGU6 (Dongle)를 BLE 모드가 아닌 기존�?� Classic 모드 ( BR/EDR) 모드로�?� 사용할수 있는지문�?�드립니다만약�? 안�?�다면, 혹시 BR/EDR �?� 지�?하는 MCU가 있는지 문�?�드립니다.�?사합니다....
Hi.I'm having hard time with my custom board based on STM32WB15CC.I referred Nucleo-WB15 schematics but using ST-Link V2 instead of ST-Link on Nucleo Board.I had an experience of STM32F411 so I thought this time I also can do it by STM32WB15. However...
I work around a project based on STM32WB55.In this project it is necessary to keep a clock / calendar when the card is off.We usually use external real time clock / calendar such as PCF85063A.I work with the core board and try to use the WB55 RTC, wi...
Hello,I have STM32WLE5CBU6 and I communicate with my Quectel chip over standard UART communication (interface LPUART, PA2, PA3) via AT commands. Transmitting from STM to Quectel is always working well, but when I want to read response from Quectel ch...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.