2024-03-06 4:26 AM
Hi to everybody.
I'm using H5 and FREE RTOS. I'm porting a project from M3 , than M4 now to H5. I used LL for all the periferals, but moving to HAL isn't a probelm (... but I prefer LL!).
On M3 and M4 I used a timers to "serve" the RTOS scheduler, then SysTick for a simple delay (yes, also on a task!). E.G. when I need few milliseconds between toggling a output while driving the display.
With H5 I can't use something like "LL_mDelay(100);" because it stuck.
How I can enable systick with H5 (voa MSX CUBE) the LL_mDelay (or HAL_Delay) to measure a time, or simply get a systick?
Thanks in advance.
Solved! Go to Solution.
2024-03-07 5:19 AM
@TheRaprus Haven't you also find the note, "When a RTOS is used, it is recommended to avoid using blocking delay and use rather osDelay"? It is quite prominent there.
2024-03-06 9:06 AM
In CubeMX configure the SYS Timebase Source to TIM1 (or some other timer (not SysTick!) you don't need for your application). Leave SysTick for FreeRTOS to use (exclusively).
2024-03-06 11:57 PM
Hi Devid.
Thanks for the answer.
Using a timer (in my case Tim5) is what I did, and also the CubeMX remeber all the time to switch fron SysTick.
WHat happe is that the HAL_Delay(x) work fine, but the LL_mDelay(x) stuck. Entering in the source of the LL (file stm32h5xx_ll_utils.c) I found this:
@note When a RTOS is used, it is recommended to avoid using blocking delay and use rather osDelay service.
void LL_mDelay(uint32_t Delay){
__IO uint32_t tmp = SysTick->CTRL; /* Clear the COUNTFLAG first */
uint32_t tmpDelay = Delay;
/* Add this code to indicate that local variable is not used */
((void)tmp);
/* Add a period to guaranty minimum wait */
if (tmpDelay < LL_MAX_DELAY)
tmpDelay++;
while (tmpDelay != 0U) {
if ((SysTick->CTRL & SysTick_CTRL_COUNTFLAG_Msk) != 0U)
tmpDelay--;
}
}The "SysTick->CTRL" is 0 and never change, so it stuck! I'll check it again to see what happen without RTOS and in HAL_Delay. I can change LL_mDelay to HAL_Delay but it'a pity!
2024-03-07 5:19 AM
@TheRaprus Haven't you also find the note, "When a RTOS is used, it is recommended to avoid using blocking delay and use rather osDelay"? It is quite prominent there.
2024-03-07 6:03 AM
Hi Pavel.
I copy the intentionally the note (and remove the others), because I know it! But as I wrote in the beginning. I used it on M3 and M4. And they work!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.