2023-01-29 2:09 AM
Using a sample example from your database code.
Compatible with stack 1.15.0 (that is the stack I am running)
STMicroelectronics ST-LINK GDB server. Version 7.1.0
Copyright (c) 2022, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.12.0
-------------------------------------------------------------------
Log output file: C:\Users\NOVODES\AppData\Local\Temp\STM32CubeProgrammer_a01928.log
ST-LINK SN : 066DFF505655806687075314
ST-LINK FW : V2J40M27
Board : P-NUCLEO-WB55
Voltage : 3.27V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x495
Revision ID : Rev Y
Device name : STM32WB5x/35xx
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M4
BL Version : 0xD5
Debug in Low Power mode enabled
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a01928.srec
File : ST-LINK_GDB_server_a01928.srec
Size : 61.74 KB
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 15]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:01.536
Verifying ...
Download verified successfully
Target is not responding, retrying...
Target is not responding, retrying...
Shutting down...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
2023-01-29 2:18 AM
And ? If your code set STOP mode on start ...
2023-01-29 2:26 AM
// APPD_Init();
what is this code? it causes it
2023-01-29 2:36 AM
Ok , better not be running the FUS I guess..
2023-01-29 4:52 AM
You dont ask question , but maybe you try debug ... APPD is aplication daemon ...
On WB firmware save energy is managed with STOP mode then you need setup debuger settings Enable debug in low power modes ENABLED seems enabled then other troubles in your app ( for example power USB overloaded, not preloaded bin firmware usw)
2023-01-29 5:47 AM
Thanks will try
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.