NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
The program size of my project is as follows "Program Size: Code=30996 RO-data=1548 RW-data=36 ZI-data=34980". The board i am using is a STM32WLJ1 board "256-Kbyte Flash memory and 64-Kbyte SRAM". I believe flash memory is causing me issues in my pro...
I just got my STM32WB55 Nucleo boards with FUS v.0.5.3 and trying to upgrade firmware but neither of the provided .bin files in "repository" ("stm32wb5x_FUS_fw.bin" or "stm32wb5x_FUS_fw_for_fus_0_5_3.bin") work. I get the same message for both when t...
I am trying to follow this video: because i think i bricked my coprocessor (m0+ ), same thing happens in two different boards.✌�? STM32WB Getting Started Series: Part 9, Stack Loading https://www.youtube.com/watch?v=wheGvdXsi4oWhen i click firmware u...
Hi All,I am getting the error FUS_STATE_IMG_NOT_AUTHENTIC while updating FUS. I am using the provided image in:STM32Cube/Repository/STM32Cube_FW_WB_V1.12.1/Projects/STM32WB_Copro_Wireless_Binaries/STM32WB5x/stm32wb5x_FUS_fw.binAs stated in the releas...
Hi everyone,I successfully setup a lora communication using the pnucleo lrwan3 kit : https://www.st.com/en/evaluation-tools/p-nucleo-lrwan3.htmlThe only thing I'm missing is the way to activate the sensor reading on the lrwan-ns1 shield. I am using t...
When I configure (with cubeMX) my BLE peripheral project to use Static Random Address or Public Address, the device is able to successfully connect and pair with a mobile device.When I change the configuration to use Resolvable Private Address, devic...
Hello,I'm working with the Nucleo board the STM32WB55 and i'm trying to send temperture data as in the eddysone tlm frame. But even I've configured the code as EddystoneTLM in the app_conf.h it is always showing up as URL beacon insteade of TLM.Can a...
I have a custom board with a quadSPI chip installed. I can program a 256-byte page just fine using HAL_QSPI_Transmit(), which I'm monitoring with a logic analyzer. But when I try to do this with HAL_QSPI_Transmit_DMA(), nothing happens on the line...
Hello, I am building an application using STM32WB55 ( 1 MB Flash) series microcontroller and planning to use BLE 5.0 to make secure connection with a device. In our use case, I am trying to compute how many keys/Bonding Info can be stored to speed up...
In STOP2 mode, the current of STM32WB5MMG is around 170uA at 3V.Using the same FW (based on the HeartRate example), the P-NUCLEO-WB55 can achieve a low current (approximately 3 uA).Is there any additional settings for STM32WB5MMG?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.