NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I want to use USB as CDC device for virtual com port along with MAC 802.15.4 FFD example code i did following steps but computer didn't detect USB device.1) I added all the files from USB_Device folder to MAC 802.15.4 FFD code.2) In middlewares adde...
Hello, Recently, I came across an exciting open-source project called ioter, which is based on the Matter thread protocol. github.com/Samsung/ioterIt appears that this project has been verified only with Thread devices based on Nordic nRF52840. Howev...
Hello everyone, I ve been trying to implement DMA ADC to ping-pong example for 5-6 days. I made HAL_ADC_PollForConversion made without problem. When I try to implement dma + adc, it return 0. I reviewed lorawan adc.c example for polling (there is no ...
We are using the STM32WLE5JCI6 chip and we are mostly done with hardware and software development but got stuck with the below issues.We are trying to read two analog inputs from PB4 (ADC1_IN3) and ADC_CHANNEL_VREFINT. (We are using a Lithium thionyl...
The first time I runned the program it worked correctly but then it doesn't work
Hello,I want to mass erase the flash of the P-NUCLEO-WB55 board using UART and USB in boot mode. I have tried mass erase using the STM32Cube programmer it is showing an error "Mass erase operation failed Please verify flash protection". All the optio...
STLINK-V3PWR Not able to connect to STM32WL and other STM32 MCU's using STM32CubeProgrammerSame MCU is working with STlink-V3 13:39:13 : ST-LINK SN : 002F004D3431510137383732 13:39:13 : ST-LINK FW : V4J2B1P4 13:39:13 : Board : STLINK-V3PWR 13:39:...
Hi all.I'm working with stm32wle5 (rak3172 module) with a custom board.It works but now I need to change default data rate DR_2 to DR_0 (need to increase distance).I have already tried to change the lines below at file RegionAU915.h//Minimal datarat...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.