2026-04-01 8:38 AM - edited 2026-04-01 8:38 AM
I'm confused by ST's seeming definition of what they think a QUAD word is....according to most of the planet a WORD is 16-bits, so a QUAD word is 64-Bits. However according to ST a quad word is 128 bits on the STM32U535.
I enclose a section of my code - essentially I want to write 11520 values which are U32's and then read them again when I power it back up, bit its getting confused because I can't get my head around whether there's 64, or 128 bits in a QUAD WORD!
xnLookup[][][] is the Parameter I want to write, and the read back which is a U32
This is the WRITE:
i=0;//Channel 0..3
j=0;//Temperature 0..180 (-50 to +130DegC)
k=0;//Term X0, X1, X2, X3 etc
n=1;//Counter for every 4th flash word
MemCount=0;//Total memory locations
//was 11520 for -50 to +130DegC. change to
for(m=0;m<11520;m++)//Total number of parameters to write - //12160
{
//Copy the polynomial term into the flash array
flashdata32[n-1].l=xnlookup[k][i][j].l;//Put the polynomial term onto the flash array
//Every 4 itterations, write the array to flash
if(n==4)
{
n=0;//reset the counter
HAL_FLASH_Program(FLASH_TYPEPROGRAM_QUADWORD, FLASH_TLOOKUP+MemCount, ((u32)flashdata32));
MemCount=MemCount+16;//Next QUAD word - 16 BYTES
}
//Do the relevant index incrementing - next temperature, next channel, or next term
if(j>=180)
{
j=0;
i++;//i is the channel number 0..3
if(i>=16)
{
i=0;
j=0;
k++;//k goes 0,1,2,3 for each polynomial term
}
}
n++;//n is the Flashword index 0..3 4 words =16 bytes
j++;//j is the temperature index
}
//Now lock the flash
HAL_FLASH_Lock();
}This is the READ:
//Read all of the configuration data
void Read_TLookup(void)
{
u16 i,j,k,l;
u32 MemCount;
l=0;
k=0;
//Read the Polynomial Calibration values
l=0;
for(k=0;k<4;k++)//Polynomial order index (X0, X1, X2, X3)
{
for(i=0;i<16;i++)//channel
{
for(j=0;j<180;j++)//temperature index - was 180, change to 190
{
MemCount=l*4;
xnlookup[k][i][j].l=*(u32*)(FLASH_TLOOKUP+MemCount);//floating point representation
l++;
}
}
}
}
Solved! Go to Solution.
2026-04-01 9:32 AM
Hello @Rob Ashworth,
A word typically denotes the native data size of a CPU, corresponding to its architecture. For example, on a 16-bit CPU, a word is 16 bits; on a 32-bit CPU, it is 32 bits, and so forth. In the case of the x86 architecture, originally a 16-bit design, the term "word" referred to 16 bits. With the evolution to 32-bit (x86) and 64-bit (x86-64) architectures, the native word size expanded accordingly to 32 bits and 64 bits, respectively, reflecting the CPU’s data handling capabilities. I hope this clarifies the misunderstanding.
Best regards,
2026-04-01 9:32 AM
Hello @Rob Ashworth,
A word typically denotes the native data size of a CPU, corresponding to its architecture. For example, on a 16-bit CPU, a word is 16 bits; on a 32-bit CPU, it is 32 bits, and so forth. In the case of the x86 architecture, originally a 16-bit design, the term "word" referred to 16 bits. With the evolution to 32-bit (x86) and 64-bit (x86-64) architectures, the native word size expanded accordingly to 32 bits and 64 bits, respectively, reflecting the CPU’s data handling capabilities. I hope this clarifies the misunderstanding.
Best regards,
2026-04-01 10:51 AM
> according to most of the planet a WORD is 16-bits, so a QUAD word is 64-Bits
The size of a "word" is dependent upon context. It is definitely not almost always 16 bits. It's generally the native size of whatever you're working with. On a 32-bit mcu, it's generally 32 bits.
Here, it is 32 bit.
2026-04-02 12:17 AM
Thanks for the reply - I guess understand even if in my view ST shouldn't have called it a "WORD" to avoid confusion.
2026-04-02 1:37 AM
Basically today "word" is equivalent to 16 bits only in Intel x86 world. When 8086 was introduced in 1979, the widest data it could handle was 16-bit, so that was called a "word".
All the computer architectures introduced after 1980 define word as 32-bit, 16-bit entity is called "halfword", and 64-bit - "doubleword". It is and was the same for MIPS, SPARC, ARM, POWER, RISC-V, ARC and Xtensa. There is no modern architecture using "word" to refer to 16-bits.
It's the architecture owner/designer who names the things - in the case of STM32 which uses ARM architecture, we should follow the ARM dictionary of names.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.