2024-11-12 11:10 PM - edited 2024-11-12 11:11 PM
Hello,
I am using a STM32WB5MMG on a custom board for a BLE application. I started the project with the Client profile. The application is able to scan and receive advertisement frames. I use a MAC filter to select on peripheral and try to connect to it. As soon as I try to connect to the server with the function aci_gap_create_connection, the program enters an infinite loop inside hci_cmd_resp_wait. The response of this particular HCI command is never received.
I don't think it is related to bad parameter value such connection interval because I already faced this issue and in this case the function aci_gap_create_connection was returning an accurate error code.
RTC is on LSE, wakeup is activated, IPCC interrupts are enabled, RFWKP is on LSE.
As suggested in another post, I monitore the SR flash register and SRAM2A first register to see if CPU2 entered Hardfault but it does not seem to.
I changed a bit hci_cmd_resp_wait and hci_cmd_resp_release to provide a timeout in case no reply is ever get from CPU2:
void hci_cmd_resp_release(uint32_t flag)
{
HW_TS_Stop(timeout_ts_ID);
UTIL_SEQ_SetEvt(1 << CFG_IDLEEVT_HCI_CMD_EVT_RSP_ID);
return;
}
void hci_cmd_resp_wait(uint32_t timeout)
{
HW_TS_Start(timeout_ts_ID, MS_TO_TICKS(timeout));
UTIL_SEQ_WaitEvt(1 << CFG_IDLEEVT_HCI_CMD_EVT_RSP_ID);
return;
}
static void TimeoutHCI(void)
{
LOG_WARNING("Timeout");
/* Affichage de l'état du coeur 2 voir AN5289 rev 18 p 40 s*/
uint32_t* ptr = SRAM2A_BASE;
LOG_DEBUG("FLASH_SR CPU2 Keyword CPU2 Link Register CPU2 stack pointer");
LOG_DEBUG("0x%08lX 0x%08lX 0x%08lX 0x%08lX 0x%08lX",FLASH->SR,*ptr, ptr[1],ptr[2],ptr[3]);
hci_cmd_resp_release(0);
}
Below is a light trace ouput to show the problem:
[app_entry.c][APPE_SysUserEvtRx][363] Wireless Firmware version 1.20.0
[app_entry.c][APPE_SysUserEvtRx][364] Wireless Firmware build 2
[app_entry.c][APPE_SysUserEvtRx][365] FUS version 1.2.0
[app_entry.c][APPE_SysUserEvtRx][367] >>== SHCI_SUB_EVT_CODE_READY
[app_entry.c][APPE_SysEvtReadyProcessing][453] >>== WIRELESS_FW_RUNNING
[app_entry.c][APPE_SysEvtReadyProcessing][477] >>== DBGMCU_GetRevisionID= 2003
[app_entry.c][APPE_SysEvtReadyProcessing][482] >>== DBGMCU_GetDeviceID= 495
[app_ble.c][APP_BLE_Init][319] Success: SHCI_C2_BLE_Init command
[app_ble.c][Ble_Hci_Gap_Gatt_Init][751] ==>> Start Ble_Hci_Gap_Gatt_Init function
[app_ble.c][Ble_Hci_Gap_Gatt_Init][764] Success: hci_reset command
[app_ble.c][Ble_Hci_Gap_Gatt_Init][778] Success: aci_hal_write_config_data command - CONFIG_DATA_PUBADDR_OFFSET
[app_ble.c][Ble_Hci_Gap_Gatt_Init][779] Public Bluetooth Address: 00:80:e1:27:9c:7c
[app_ble.c][Ble_Hci_Gap_Gatt_Init][792] Success: aci_hal_write_config_data command - CONFIG_DATA_IR_OFFSET
[app_ble.c][Ble_Hci_Gap_Gatt_Init][805] Success: aci_hal_write_config_data command - CONFIG_DATA_ER_OFFSET
[app_ble.c][Ble_Hci_Gap_Gatt_Init][818] Success: aci_hal_set_tx_power_level command
[app_ble.c][Ble_Hci_Gap_Gatt_Init][831] Success: aci_gatt_init command
[app_ble.c][Ble_Hci_Gap_Gatt_Init][867] Success: aci_gap_init command
[app_ble.c][Ble_Hci_Gap_Gatt_Init][906] Success: aci_gap_set_io_capability command
[app_ble.c][Ble_Hci_Gap_Gatt_Init][934] Success: aci_gap_set_authentication_requirement command
[app_ble.c][Ble_Hci_Gap_Gatt_Init][949] Success: aci_gap_configure_whitelist command
[app_ble.c][Ble_Hci_Gap_Gatt_Init][952] ==>> End Ble_Hci_Gap_Gatt_Init function
[app_ble.c][APP_BLE_Init][352] Success: aci_hal_set_radio_activity_mask command
[app_ble.c][APP_BLE_Init][354]
[p2p_client_app.c][P2PC_APP_Init][169] -- P2P CLIENT INITIALIZED
[app_ble.c][Scan_Request][972]
** START GENERAL DISCOVERY (SCAN) **
[...]
[DBG] main:164 >FLASH_SR CPU2 Keyword CPU2 Link Register CPU2 stack pointer]
[DBG] main:165 >0x00080000 0x20030028 0x20030048 0x20030058 0x20030078]-- GAP GENERAL DISCOVERY PROCEDURE_COMPLETED
** CREATE CONNECTION TO SERVER **
[WARNING] TimeoutHCI:1092 >Timeout]
[DBG] TimeoutHCI:1095 >FLASH_SR CPU2 Keyword CPU2 Link Register CPU2 stack pointer]
[DBG] TimeoutHCI:1096 >0x00080000 0x20030028 0x20030048 0x20030058 0x20030078]
[WARNING] TimeoutHCI:1092 >Timeout]
[DBG] TimeoutHCI:1095 >FLASH_SR CPU2 Keyword CPU2 Link Register CPU2 stack pointer]
[DBG] TimeoutHCI:1096 >0x00080000 0x20030028 0x20030048 0x20030058 0x20030078]
[WARNING] TimeoutHCI:1092 >Timeout]
[DBG] TimeoutHCI:1095 >FLASH_SR CPU2 Keyword CPU2 Link Register CPU2 stack pointer]
[DBG] TimeoutHCI:1096 >0x00080000 0x20030028 0x20030048 0x20030058 0x20030078]
[WARNING] TimeoutHCI:1092 >Timeout]
[DBG] TimeoutHCI:1095 >FLASH_SR CPU2 Keyword CPU2 Link Register CPU2 stack pointer]
[DBG] TimeoutHCI:1096 >0x00080000 0x20030028 0x20030048 0x20030058 0x20030078]
[WARNING] TimeoutHCI:1092 >Timeout]
[DBG] TimeoutHCI:1095 >FLASH_SR CPU2 Keyword CPU2 Link Register CPU2 stack pointer]
[DBG] TimeoutHCI:1096 >0x00080000 0x20030028 0x20030048 0x20030058 0x20030078]
[WARNING] TimeoutHCI:1092 >Timeout]
[DBG] TimeoutHCI:1095 >FLASH_SR CPU2 Keyword CPU2 Link Register CPU2 stack pointer]
[DBG] TimeoutHCI:1096 >0x00080000 0x20030028 0x20030048 0x20030058 0x20030078]
And then below is the full trace with the following debug parameters:
#define TL_HCI_CMD_DBG_EN 1 /* Reports BLE command sent to CPU2 and the command response */
#define TL_HCI_CMD_DBG_RAW_EN 0 /* Reports raw data BLE command sent to CPU2 and the command response */
#define TL_HCI_EVT_DBG_EN 1 /* Reports BLE Asynchronous Events received from CPU2 */
#define TL_HCI_EVT_DBG_RAW_EN 0 /* Reports raw data BLE Asynchronous Events received from CPU2 */
#define TL_MM_DBG_EN 1 /* Reports the information of the buffer released to CPU2 */
[DBG] SVCCTL_App_Notification:634 >Rx adv from 8C:A6:82:E0:00:10]
[tl_mbox.c][OutputDbgTrace][700] mm evt released: 0x3E
[tl_mbox.c][OutputDbgTrace][701] buffer addr: 0x20030238
[tl_mbox.c][OutputDbgTrace][705]
[tl_mbox.c][OutputDbgTrace][758] ble evt: 0x3E
[tl_mbox.c][OutputDbgTrace][761] payload: 02 01 04 01 C8 1D E7 CB 9A 35 00 9F
[tl_mbox.c][OutputDbgTrace][776]
[tl_mbox.c][OutputDbgTrace][700] mm evt released: 0x3E
[tl_mbox.c][OutputDbgTrace][701] buffer addr: 0x20030200
[tl_mbox.c][OutputDbgTrace][705]
[tl_mbox.c][OutputDbgTrace][767] ble evt: 0xFF
[tl_mbox.c][OutputDbgTrace][768] subevtcode: 0x0407
[tl_mbox.c][OutputDbgTrace][771] payload: 02 00 00
[tl_mbox.c][OutputDbgTrace][776]
[app_ble.c][SVCCTL_App_Notification][430] -- GAP GENERAL DISCOVERY PROCEDURE_COMPLETED
[tl_mbox.c][OutputDbgTrace][694] mm evt released: 0xFF
[tl_mbox.c][OutputDbgTrace][695] subevtcode: 0x0407
[tl_mbox.c][OutputDbgTrace][696] buffer addr: 0x20030200
[tl_mbox.c][OutputDbgTrace][705]
[app_ble.c][Connect_Request][995]
** CREATE CONNECTION TO SERVER **
[DBG] Connect_Request:1001 >FLASH_SR CPU2 Keyword CPU2 Link Register CPU2 stack pointer]
[DBG] Connect_Request:1002 >0x00000000 0x20030028 0x20030048 0x20030058 0x20030078]
[tl_mbox.c][OutputDbgTrace][710] ble cmd: 0xFC9C
[tl_mbox.c][OutputDbgTrace][713] payload: 20 03 20 03 00 10 00 E0 82 A6 8C 00 28 00 50 00 00 00 F4 01 10 00 10 00
[tl_mbox.c][OutputDbgTrace][716]
[WARNING] TimeoutHCI:1096 >Timeout]
[DBG] TimeoutHCI:1099 >FLASH_SR CPU2 Keyword CPU2 Link Register CPU2 stack pointer]
[DBG] TimeoutHCI:1100 >0x00080000 0x20030028 0x20030048 0x20030058 0x20030078]
[WARNING] TimeoutHCI:1096 >Timeout]
[DBG] TimeoutHCI:1099 >FLASH_SR CPU2 Keyword CPU2 Link Register CPU2 stack pointer]
[DBG] TimeoutHCI:1100 >0x00080000 0x20030028 0x20030048 0x20030058 0x20030078]
[WARNING] TimeoutHCI:1096 >Timeout]
[DBG] TimeoutHCI:1099 >FLASH_SR CPU2 Keyword CPU2 Link Register CPU2 stack pointer]
[DBG] TimeoutHCI:1100 >0x00080000 0x20030028 0x20030048 0x20030058 0x20030078]
Any help on this subject would be greatly appreciated.
Solved! Go to Solution.
2024-12-10 3:00 AM
After deeper investigations, we managed to fix the issue, though I do not understand clearly why, the issue disappears if RNG is deactivated OR "clock error detection" in RNG is disabled.
I do not think that we will require RNG module in our project, so I am fine to live with this.
Any insight regarding the reasons behind would still be appreciated.
Best regards
2024-11-21 4:24 AM
Up.
Sorry about this but we are stuck on this for a couple of months..
2024-11-25 12:14 AM
Hello @BBute.1
Could you try to reproduce this behavior on the STM32WB5MM-DK.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-25 1:42 AM
Hello,
I already did and I got the exact same behaviour.
Thanks for your help,
Best regards,
2024-11-25 7:22 AM
Hello @BBute.1
For more investigation I've escalated your request internally (under internal ticket number 196955). We will try to be back to you ASAP.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-12-06 6:07 AM
Hi BBute.1,
I've just done the test on my side with a “p2pClient” on the STM32WB5MMG starting from release v1.20.0.
I don't reproduce the problem you encountered.
Would it be possible for you to share with us your project running on DK please?
BR, Joé
2024-12-10 3:00 AM
After deeper investigations, we managed to fix the issue, though I do not understand clearly why, the issue disappears if RNG is deactivated OR "clock error detection" in RNG is disabled.
I do not think that we will require RNG module in our project, so I am fine to live with this.
Any insight regarding the reasons behind would still be appreciated.
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.