2019-07-18 7:51 PM
Hi All,
I have trouble getting the BlE working on my new hardware(stm32wb55RGV6). The prgram can't enter into
APP_BLE_Init( ); . The same code in P-NUCLEO-WB55.Nucleo(stm32wb55RGV6U)
can work. What's different between stm32wb55RGV6 and stm32wb55RGV6U?
2019-08-22 9:16 AM
You can also check whether the SFSA value is consistent with the SBRV value.
For my own current downloaded example (Using the V1.2.0 WB FW package), the SFSA is 0xCB while the SBRV is 0x32C00.
For SFSA, it is an offset aligned on a 4K boundary starting from the start address of the Flash memory (0x0800000) => 0x080CB000
For SBRV, it is a word aligned value also starting from the start address of the Flash memory =>0x32C00x 4 = 0xCB000 real offset => 0x080CB000
So both values are coherent leading to the same address pointing on the same location in the Flash area.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.