2026-04-09 8:19 PM
Hi,
Our product uses 2 x STM32WB55 MCUs, where one as Server/Coordinator and the other one as Client/Router for Zigbee. However, our customer prefer to use customized PAN ID or Extended PAN ID so that more controllable and traceable by their application software later. Below is the setup of the Server/Coordinator and Client/Router in my firmware (modify based on sample code "Zigbee_OnOff_Server_Coord & Zigbee_OnOff_Client_Router").
** Server/Coordinator :
startupControl = ZbStartTypeForm;
config.panId = 0x0001; // range from 0x0001 to 0xfffe
config.extendedPanId = 0x00001; // incremental from 0x01 onwards
** Client/Router:
startupControl = ZbStartTypeRejoin;
config.panId = 0x0001; // range from 0x0001 to 0xfffe
config.extendedPanId = 0x00001; // incremental from 0x01 onwards
Questions:
1. May I know the configuration above is enough and valid to do so?
2. What are the steps needed or I missed out in order to use customized PAN ID or extended PAN ID or even the short address if question 1 above is not valid and enough?
3. How to bypass the default auto PAN ID or extended PAN ID assignment by wireless stack?
4. Do I need to rebind my client/router with the server/coord after changing the PAN ID on client/router to match server/coord's PAN ID?
5. Under what circumstances we need to do binding? during pairing? and only once will do?
Thanks.
Solved! Go to Solution.
2026-04-16 7:01 AM
Hi @Phang,
Please find a snippet code below showing how to fix the Extended address for a Zigbee device :
/* Fixed 64-bit IEEE address - must be unique for each device */
static const uint64_t g_ieee_addr = 0x00124B000025AA11ULL;
void APP_ZIGBEE_Init(void)
{
struct ZbInitT *zb_init;
zb_init = ZbInit(g_ieee_addr, NULL, NULL);
if (zb_init == NULL) {
APP_DBG("ZbInit failed\r\n");
return;
}
APP_DBG("Zigbee stack initialized with fixed IEEE address: 0x%016llX\r\n",
(unsigned long long)g_ieee_addr);
}
Regards,
Ouadi
2026-04-09 8:30 PM
Added from my previous post above, I have implemented persistent data NVM in both Serve/Coord and Client/Router and it is working well with auto PAN ID but unfortunately not with my custom PAN ID especially after unplug/plug back the server/coord device from USB port.
2026-04-13 7:36 AM
Hi @Phang,
Thanks for contacting us through the support community channel, please find the answers to your questions :
Best regards,
Ouadi
2026-04-13 9:32 PM
Hi Ouadi,
Thanks for the reply. The reason I asked these questions because our customer's existing product requires user to set 4/5 bytes server/coord ID onto the client device once in order to allow to join/form the network. So, they wanted this feature in their new product design for Zigbee as well so that they can control, trace and monitor connected devices.
Other than using the PANID and/or Ext PANID method, any other way can be used instead? This is because I ever seen the custom PANID and Ext PANID set inside the server/coord's persistent data NVM get changed but still able to receive data from clients.
2026-04-14 3:43 AM
Hi Phang,
If I understand the concern correctly, the customer is looking for a user-configurable identifier to be provisioned from the coordinator side for each joining device, so that the application can later use this identifier for control, traceability, and monitoring, correct?
For such a use case, the most appropriate identifier is the device’s IEEE address. This is a 64-bit globally unique address that is stable and well suited for:
At startup, the joining device can provide its own extended IEEE address through the Zigbee initialization flow, e.g: ZbInit(). This address can then be provisioned or registered on the coordinator side, allowing the coordinator application to use it for filtering, validation, and traceability.
I hope this answers the question.
Regards,
Ouadi
2026-04-14 4:51 AM
Hi Ouadi,
Yes, your understanding is correct. So, do you have sample code for using extended IEEE address or what should I start for coord and router? Can you provide in more details info /step?
Thanks.
2026-04-16 7:01 AM
Hi @Phang,
Please find a snippet code below showing how to fix the Extended address for a Zigbee device :
/* Fixed 64-bit IEEE address - must be unique for each device */
static const uint64_t g_ieee_addr = 0x00124B000025AA11ULL;
void APP_ZIGBEE_Init(void)
{
struct ZbInitT *zb_init;
zb_init = ZbInit(g_ieee_addr, NULL, NULL);
if (zb_init == NULL) {
APP_DBG("ZbInit failed\r\n");
return;
}
APP_DBG("Zigbee stack initialized with fixed IEEE address: 0x%016llX\r\n",
(unsigned long long)g_ieee_addr);
}
Regards,
Ouadi
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.