cancel
Showing results for 
Search instead for 
Did you mean: 

Does the B-L072Z-LRWAN1 support I2C in both slave/master mode.

JAnth
Associate

I wish to connect this kit (STM32L072CZY6TR) to a raspberry pi. As the Pi only supports SPI in master mode I need to use I2C to get a two way conversation.

I wish to send and receive the occasional codes from a server via LORAWAN and communicate those to a Raspberry Pi which in turn will control machinary. It is impossible for the Pi to be connected to the internet. I am hoping to not have to go down the GSM route.

Many thanks

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

It will do whatever you program into it. You'll have to write the I2C support code.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.