STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

How To Connect Your First LoRa Device ( STM32L072CZ Microcontroller ) Using B-L072Z-LRWAN1 And The Shield X-NUCLEO-IKS01A2 From STMicroelectronics

Hello , Today I Wrote My Second Article Entitled How To Connect Your First LoRa Device ( STM32L072CZ Microcontroller ) . In This Project i used The B-L072Z-LRWAN1 Development Board From STMicroelectronics and Also the Shield X-NUCLEO-IKS01A2 From STM...

Resolved! RTC clock ticking faster than actual.

Hello everyone,I am currently developing a code for my custom board that has BLE communication along with RTC and timer(PWM) initialized. I am currently testing my code first on the PNucleoWB55 development board. The issue is that the normal RTC_Alar...

AKetc by Associate III
  • 4192 Views
  • 5 replies
  • 0 kudos

Resolved! Why I can't received a message downlink immediately?

Hi All;​ I am use I-CUBE-LRWAN version 1.2.1. I am program in class C mode. I send a message downlink from network server and I checked that the data was actually sent out. Why I can't received a message downlink immediately. Could you please adv...

Gz by Senior
  • 1148 Views
  • 1 replies
  • 0 kudos

Can SAI and BLE used together in one application?

I am using STM32l476RG nucleo board and X_Nucleo_IDB051.I want to transfer SAI peripheral data over BLE.I have tried to generate code using CUBEMX but device fails to advertise as well as it is fails to capture data over SAI.Alone SAI example is work...

Skand.19 by Associate
  • 854 Views
  • 0 replies
  • 0 kudos

After the new firmware package for STM32WB, v1.2, I am not able to see the STM32WB on COM port after running a simple USB CDC code to enable serial communication.

//main.c file /* Includes ------------------------------------------------------------------*/ #include "main.h" #include "usb_device.h" #include "gpio.h"   /* Private includes ----------------------------------------------------------*/ /* USER CODE...

HSing by Associate II
  • 1409 Views
  • 2 replies
  • 1 kudos

About the wireless stack downloaded by default

Hi,expert.I am learning to use P-NUCLEO to support development using STM32WB.As the title, I have a question about the wireless stack.I learned in UM2550 that when writing a wireless stack, the current wireless stack needs to be erased and written ag...

ota-s by Associate II
  • 2145 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.