cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WB5 BLE

stop
Associate II

Hi all,

no experience, so please explain like to a child.

I want to jump into digital.

My idea is to make a bluetooth speaker with LED meter so:

USB C for Power(CYBD3177) and/or Audio IN(STM32wb5).

Bluetooth Audio IN (STM32WB5) -> out to Class D Amp (TAS5827)

Two more Data Lines to control WS2812B

Which physical connections do I need?

I guess:

  • D+D- from USB C to STM32
  • DIN L/R (GPIOs?) from STM32 to WS2812
  • I2S(LRCLK,SCLK,SDIN) from STM32 to TAS5827
  • 4 more eventually Data lines (GPIOs?) from TAS 5827 to STM32 for return messages

is this correct?

thanks

 

1 ACCEPTED SOLUTION

Accepted Solutions
Andrew Neil
Super User

@stop wrote:

no experience


No electronics? No programming at all? No microcontrollers?

 


@stop wrote:

so please explain like to a child.


As with a child getting started,  it would be wiser to start with something simpler!

Begin with the basics, then move up to more advanced stuff.

Here are some beginner's getting started tips:

https://www.avrfreaks.net/s/topic/a5C3l000000UYGFEA4/t145493?comment=P-1392529

 


@stop wrote:

My idea is to make a bluetooth speaker with LED meter 


That's a pretty advanced project for a beginner!

Be aware that most "Bluetooth speakers" use Bluetooth Classic - and none of the STM32s support that:

https://community.st.com/t5/stm32-mcus-wireless/stm32-bluetooth-classic-mcu/m-p/700352/highlight/true#M20355 

https://community.st.com/t5/stm32-mcus-wireless/classic-bluetooth-in-stm32wba55/m-p/694980/highlight/true#M20091

https://community.st.com/t5/stm32-mcus-wireless/stm32wba55g-dk1-not-compatible-with-all-mobiles/m-p/700350/highlight/true#M20354

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

View solution in original post

4 REPLIES 4
Andrew Neil
Super User

@stop wrote:

no experience


No electronics? No programming at all? No microcontrollers?

 


@stop wrote:

so please explain like to a child.


As with a child getting started,  it would be wiser to start with something simpler!

Begin with the basics, then move up to more advanced stuff.

Here are some beginner's getting started tips:

https://www.avrfreaks.net/s/topic/a5C3l000000UYGFEA4/t145493?comment=P-1392529

 


@stop wrote:

My idea is to make a bluetooth speaker with LED meter 


That's a pretty advanced project for a beginner!

Be aware that most "Bluetooth speakers" use Bluetooth Classic - and none of the STM32s support that:

https://community.st.com/t5/stm32-mcus-wireless/stm32-bluetooth-classic-mcu/m-p/700352/highlight/true#M20355 

https://community.st.com/t5/stm32-mcus-wireless/classic-bluetooth-in-stm32wba55/m-p/694980/highlight/true#M20091

https://community.st.com/t5/stm32-mcus-wireless/stm32wba55g-dk1-not-compatible-with-all-mobiles/m-p/700350/highlight/true#M20354

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Just new to microcontroller.

What do you mean by bluetooth classic?

stop
Associate II

oh I got it thanks

 

stop
Associate II

@Andrew Neil 

Do you say that with STM32 I cannot receive audio via Bluetooth and send it via I2S to a Class D amp?

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.