2019-01-24 7:23 AM
Hi,
I use the b-l072z-lrwan1 to make lora advertisment and it's work.
I use the project AT_slave or END_Node.
But i want to use the second uart USART1 and nothing work in the environment.
If i just change the file B-L072Z-LRWAN1\Applications\LoRa\End_Node\Core\inc\mlm32l0xx_hw_conf
The program launch but nothing appear on the UART.
I make a project with 2 UART with STM32CubeMX and both work great (it's not a hardware problem)
Someone could help me?
Solved! Go to Solution.
2019-01-28 5:19 AM
Ok, will let them manage this then.
2019-01-28 5:23 AM
Thank you I remember this table but I did not make the link.
Read in RM0377 rev8. p246.
I will re-read this part again to find a solution to my problem...
EDIT : a good tutorial for this problem :
2019-01-28 5:24 AM
If you could continue help me that could be great.
Because the reactivity is really better here.
EDIT :
I have USART2 working and USART1 sending only the first message. (DMA locked somewhere?)
i just comment these ligns that i'va put when i init my USART 2 :
/* NVIC for USART, to catch the TX complete */
//HAL_NVIC_SetPriority(USART2_IRQn, 1, 1);
//HAL_NVIC_EnableIRQ(USART2_IRQn);
2019-01-29 1:39 AM
@Community member
Do you have an idea where a can found a project with lora installed and 2 USART 115200?
When i change the baudrate in AT_slave project, the RX part stop working...
2019-01-29 9:13 AM
My application with the Murata module uses multiple USART, I have no specific need to port the AT_Slave application. Getting a working port built and tested would take some time/effort. You might need to refactor the code to deal with high baud rates, and timeouts associated with the LoRa stack.
2019-01-31 12:05 AM
I already tried to start from a fresh project.
The USART work well but incorporate the lora stack is not so easy....
My prototype will be ready next week, so i have to go forward and i use the program AT_slave with 9600baud...
I have no specific need of the AT_slave application too. But i need a project with a functionnal UART in full duplex mode and lora stack...
2019-02-01 3:04 AM
@Community member
Lora work here. Start to a fresh program that's look good.
I have my 2 UART in TX RX mode.
But the lora.c of the example is really different from the lora.c from the lora stack and i have some trouble.
The problem is when i send an downlink frame, it take 8 uplink to be send.
In the example every uplink allow a downlink.
2019-02-05 6:32 AM
Hi @Community member ,
I'm not really happy with my CubeMX project because Lora does not work very well ...
So get back with EndNode project.
Lora is OK
I have TX and RX on UART2 at 115200 !!
But when i tried to initialize USART1
// if(HAL_UART_Init(&huart1) != HAL_OK)
// {
// /* Initialization Error */
// Error_Handler();
// }
My USART_2 gState still locked in HAL_UART_STATE_BUSY_TX mode.
I don't understand where the default is.
I only change this comment lign and USART2 stop working.
The DMA not release the gState in READY mode...
Do you have an idea?
2019-02-14 4:44 AM
the solution is found :
HAL_UART_MspInit and HAL_UART_MspDeInit shall be separated depending on wich huart called.
void HAL_UART_MspInit(UART_HandleTypeDef *huart)
{
static DMA_HandleTypeDef hdma_tx;
if(huart->Instance==USART1)
{
__USART1_CLK_ENABLE();
__GPIOA_CLK_ENABLE();
vcomh1_IoInit();
//HAL_NVIC_SetPriority(USART1_IRQn, USARTx_DMA_Priority, 1);
//HAL_NVIC_EnableIRQ(USART1_IRQn);
}
else
{
void HAL_UART_MspDeInit(UART_HandleTypeDef *huart)
{
if(huart->Instance==USART1)
{
vcomh1_IoDeInit( );
__USART1_FORCE_RESET();
__USART1_RELEASE_RESET();
}
Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.