NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
HelloI m Electronics engineer in Turkey.I m designing bluetooth controlled led lamb. It must be controlled by phone ios and android. And it must connect each other.Would you advise me a module and application
Hi,I use the b-l072z-lrwan1 to make lora advertisment and it's work.I use the project AT_slave or END_Node.But i want to use the second uart USART1 and nothing work in the environment.If i just change the file B-L072Z-LRWAN1\Applications\LoRa\End_Nod...
I have a combination of a Nucleo64 (STM32L053) with an X-NUCLEO-S2868AI S2-LP board.The program on it works fine, now I want to test to power from a battery. 3.6V I took out the jumpers that connect the processor to the ST-Link section, only the uart...
BS"DHi,I am new in the Lora world. I have the ST Lora EVAL(B-L072Z-LRWAN1) boards and I downloaded from ST the Software examples. One of them is the Ping-Pong application. The thing is that the application works, but after a time the receiver stops w...
Hello,I am using 'B-l072z-lrwan1' EV kit to join server of LoRaWAN through gateway.I understand where to use APPKEY and APPEUI provided by gateway server of LoRaWAN. But the EV kit do not join to server. I refer to example embedded code in 'https:...
I have a STm32WB55 Nucleo Pack with me, I am using MAC High Sierra 10+. Can you tell me the steps to get started or point out the right place to look for. I am very new to ST environment .Regards,Prasad.
Hello everyone!First let me introduce myself. I am an IT engineer from a company CREA Plus that is stationed in Ljubljana, Slovenia. I got assigned a project, that uses the STM32F100 chips.As I have no experience myself and am only getting informatio...
Hello, I use two Evaluation boards STEVAL-FKI433V2 and now there is a task to order simpler and more compact PCB. The STEVAL-FKIxxx Gerber archive https://www.st.com/resource/en/board_manufacturing_specification/steval-fki433v2_gerber.zipincludes the...
Hi, I trying to use an STM21L073 Nucleo-64 with my custom board LoRa (SX1261). I use your code I CUBE LRWAN version 1.2.1. At this time I can see JOIN procedure start. The node send a request JOIN to our GW and GW send a Accept JOIN. But in Tera Term...
I am using LORAWAN and after I joined as OTA, how to join as ABP using the generated season keys which generated after joined OTA?I read before thatits better first to join as OTA then join as ABP using the generated keys.Also, how to change the TX d...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.