2022-04-26 7:26 AM
Hello everyone,
I want to make a project with STM32L series and LORA module and battery optimization is essential. I am going to run MCU under 1.8V but I am still not sure about LORA module. I am seeing support 1.8V operational mode. I assume if I have any problem 1.8V I will switch it to 3V3. In this scenerio, 1V8 stm32l0 and 3V3 Lora communicates with SPI and Lora spi will be 3V3. Can the stm32l0 handle the 3V3 spi com. Any person available here who is experienced about with 1V8.
Thanks in advance.
Solved! Go to Solution.
2022-04-28 3:14 AM
"I thought maybe I missed the important point on reference manuel like 1.8V has different working condition"
You need to look in the Datasheet (rather than Reference Manual) - that's where you will find electrical characteristics.
If the question's now answered, please mark the solution:
2022-04-26 11:09 AM
What LoRa module, exactly ?
You will have to check the LoRa module documentation to see if it is compatible with 1.8V.
Why not just use a level-shifter chip?
2022-04-27 1:05 AM
Hi Andrew,
1 - I cant use level shifter by extra cost
2- I have read the docs and STM32L and lora support 1.8V. just this is my first experience in this voltage level and we are designing the board for 1.8V I hope it is ok. Also I checked it to ask someone yesterday(after posting this question again here)who has experience in lora module (hopeRF) told me it is ok. and also this circuit has lsm6dso, low power is important. As much as I see that is ok.
2022-04-27 2:48 AM
"I have read the docs and STM32L and lora support 1.8V"
So where's the problem?
2022-04-27 11:58 PM
So no problem now, I post the question before I got the answers from someone, but maybe someone like me want to be sure reading this post. I thought maybe I missed the important point on reference manuel like 1.8V has different working condition. iks01a3 has level shifter and this made me doubt. That is it. Thanks for answers.
2022-04-28 3:14 AM
"I thought maybe I missed the important point on reference manuel like 1.8V has different working condition"
You need to look in the Datasheet (rather than Reference Manual) - that's where you will find electrical characteristics.
If the question's now answered, please mark the solution:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.