STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! Exit Standby-Mode with RTC-Alarm after using BLE

Hello people,I am working on a Project with the stm32wb55 which includes Low Power Modes (Standby) and Bluetooth (BLE).When i turn off the Bluetooth part the controller can simply enter and exit Standbymode by my choice.However if i activate BLE on a...

Aok.1 by Associate
  • 1448 Views
  • 1 replies
  • 0 kudos

STM32WB BLE not working

Hello , I am fairly new to microcontroller programming and sorry if this is a noob question. I have a STM32WB55RG board and I want to learn developing a BLE application. I did an example from STM Workshop (Hands On) and it worked very well. Then i tr...

STM32WB Can't Use NOTIFY after OTA update without power reset

Hello!I'm trying to use the base OTA firmware updater within the STM32WB github package.For some reason, when I try to use the notify characteristic in my app after an OTA update, the notifications aren't being sent out.Is there something that needs ...

WSher.1 by Associate II
  • 1843 Views
  • 2 replies
  • 0 kudos

How to enable notification in P2P client?

Hi,I am using STM32WB55 USB dongle board as a client and another STM32WB55 USB dongle board as server. I want to send data from server to client using notify characteristic. How to enable notification in the client to receive the data ?

SChan.8 by Associate II
  • 1429 Views
  • 1 replies
  • 1 kudos

Resolved! IAR EWARM Templates or examples for STM32WL ?

Hello,I have bought a devkit NUCLEO-WL55JC2. I'm looking for an IAR EWARM template project or examples. Someone knows where i can find it? I find only examples running under CUBEIDE.Thanks !:grinning_face:

STM32WL55 RF power amplifier impedance

Dear all,I need to design a custom board for LoRa 868MHz network. The AN5457 provides the design example considering the +22 dBm (when using RFO_HP) or +14 dBm (when using RFO_LP)) with UFQFPN48 package.Also, the output impedance is reported for diff...

0693W00000JNI0BQAX.png 0693W00000JNHuDQAX.png
frnt by Senior
  • 3689 Views
  • 5 replies
  • 1 kudos
IKas.1 by Associate II
  • 1070 Views
  • 1 replies
  • 0 kudos

stm32wl55- No device found on target

Hello everyone. I am working with nucleo-wl55jc1 (with stm32wl) and i have a problem. When i try to download a program in cortex m4 i can make it succesfully. But when i try to download a program in cortex m0+ , debugging is unsuccesful. "Failed to s...

IKas.1 by Associate II
  • 1913 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.