cancel
Showing results for 
Search instead for 
Did you mean: 

Is the reduced power comsumption the only advantage of using the RFO_LP output respect RFO_HP? Can I use the same RF matching network for RFO_LP and RFO_HP outputs? Any disadvantage of using the same RF matching network for both outputs?

AZube.2
Associate III

I am developing a hardware design using the STM32WLE5JCI6. As a reference, I am looking at projects "MB1842.PrjPcb" (reference design) and "MB1389.PrjPcb" (Nucleo-WL55JC1 design files)

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Benoit MARCHAND
ST Employee

Hello,

Basically, yes, "only" advantage of using RFO_LP is to reduce current consumption. But this adavantage is huge if you are working on battery.

2nd advantage is to be able to set RF Output Power between -10 and -17dBm.

If you're not on battery and don't care current consumption and need to support different RF Output Powers below and above 15dBm, then you can decide to use only RFO_HP.

If you need to use both RFO_LP and RFO_HP, then you need 2 matching networks (you cannot connect RFO_LP and RFO_HP to a single matching network). As these 2 outputs have different impedances, it is far better for RF output power and current power consumption to use specific matching network BOMs for each of the outputs.

Hope this clarifies.

BR,

Benoit

View solution in original post

2 REPLIES 2
Benoit MARCHAND
ST Employee

Hello,

Basically, yes, "only" advantage of using RFO_LP is to reduce current consumption. But this adavantage is huge if you are working on battery.

2nd advantage is to be able to set RF Output Power between -10 and -17dBm.

If you're not on battery and don't care current consumption and need to support different RF Output Powers below and above 15dBm, then you can decide to use only RFO_HP.

If you need to use both RFO_LP and RFO_HP, then you need 2 matching networks (you cannot connect RFO_LP and RFO_HP to a single matching network). As these 2 outputs have different impedances, it is far better for RF output power and current power consumption to use specific matching network BOMs for each of the outputs.

Hope this clarifies.

BR,

Benoit

AZube.2
Associate III

Hello,

Unsderstood, thank you for the answer!

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.