cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-WL55JC frequency range confusion

sboucher78
Associate II

Hi,

There is confusion with NUCLEO-WL55JC frequency range. Maybe 2 distinct Web pages should be considered for NUCLEO-WL55JC1 and NUCLEO-WL55JC2.

Board pagehttps://www.st.com/en/evaluation-tools/nucleo-wl55jc.html

Frequency range indicated: 150 MHz to 960 MHz (none JC1 or JC2 precision, as there were only one model)

AN5406 - How to build a LoRa® application with STM32CubeWL

Frequency range indicated for NUCLEO-WL55JC2 at page 7: 470 MHz and 520 MHz

Frequency range indicated for NUCLEO-WL55JC1 at page 7: 865 MHz and 930 MHz

UM2592 - STM32WL Nucleo-64 board (MB1389)

Frequency range indicated for NUCLEO-WL55JC2 at page 3: 433 to 510 MHz

Frequency range indicated for NUCLEO-WL55JC1 at page 3: 865 to 928 MHz

What is the real frequency range of NUCLEO-WL55JC2 and NUCLEO-WL55JC1?

When I bought the boards, I did not pay attention to the JC2 precision, since I wanted a 915 MHz frequency band as it is indicated in the board page. I lost a lot of time struggling with the Cube examples that did not work because I configured it to work with 915 MHz.

1 ACCEPTED SOLUTION

Accepted Solutions
Issamos
Lead III

Hello @sboucher78 

For the frequency range of both evaluation boards. I think each board should work on both frequency ranges (from AN5406 and UM2592) since there is not a big difference between both ranges. But the correct range should be the one on the UM2592. I think both documents should have the same values. @Imen.D could you please have a look at this. 
Both boards are based on the same MCU but with different HW RF configuration to be compatible with LB (Low-Band) or HB (High-Band). So, using a frequency that is not on the supported band may work but with Low RF performance. For the webpage, I think your suggestion may be considered by the Marketing team in ST. But a webpage for both boards with a clear note that mention the difference between both boards revisions should be fine. I agree with you that this may be confusing. 
Best Regards.

II

View solution in original post

3 REPLIES 3
Issamos
Lead III

Hello @sboucher78 

For the frequency range of both evaluation boards. I think each board should work on both frequency ranges (from AN5406 and UM2592) since there is not a big difference between both ranges. But the correct range should be the one on the UM2592. I think both documents should have the same values. @Imen.D could you please have a look at this. 
Both boards are based on the same MCU but with different HW RF configuration to be compatible with LB (Low-Band) or HB (High-Band). So, using a frequency that is not on the supported band may work but with Low RF performance. For the webpage, I think your suggestion may be considered by the Marketing team in ST. But a webpage for both boards with a clear note that mention the difference between both boards revisions should be fine. I agree with you that this may be confusing. 
Best Regards.

II


@Issamos wrote:

I think both documents have the same values.


Thanks to Issamos et Andrew Neil for you quick responses. I think both documents should have the same values, but it is not the case since I copied the values from those documents. It would be reassuring if both documents showed the same values.

 


@Issamos wrote:

For the webpage, I think your suggestion may be considered by the Marketing team in ST. But a webpage for both boards with a clear note that mention the difference between both boards revisions should be fine.


A clear note indicating the difference between the two cards would suffice and would avoid confusion. I hope that ST's marketing department will make this addition.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.