2025-10-15 11:18 PM
Hello,
I am currently testing Bluetooth LE communication between two STM32WB5MM-DK boards. For the test, I am using
the data_throughput example, which I've adapted from the P-NUCLEO-WB55 software package.
According to the official datasheet for the STM32WB5MMG module, the "Features" section mentions a
communication range of "up to 75 meters."
However, in my real-world tests, I am only achieving a stable connection range of about 10 meters. My test
conditions are as follows:
* TX Power: +6 dBm (the maximum setting)
* TX PHY: 1 Mbps
This significant difference between the datasheet specification and my results leads to two main questions:
1. Are there any recommended methods to increase the communication range using this same hardware setup
(STM32WB5MM-DK)? For example, are there specific software configurations or best practices I might be missing?
2. Under what specific test conditions was the "up to 75 meters" range validated by ST? Understanding the test
environment (e.g., open-air, line-of-sight, PHY used) would be very helpful for me to manage my expectations
and design accordingly.
Any advice or insights on this matter would be greatly appreciated.
Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.