2023-11-14 3:57 AM
Hello ,
I'm using the Nucleo-WL55JC1 in my project as Gateway and End-devices.
The SW Works well and it communicate properly, but i have problem with the RANGE between the Gateway and the End-device.
Know when I change the Antenna I can communicate with 300metres as range , but i like to achieve more distances like 1Km or +
Actual SW Params :
SP = 12
TxPower = 22db
Bandwidth = 125khz.
How can I increase the range , in SW or HW side ?
Thank you in advance.
2023-11-14 6:03 AM - edited 2023-11-14 6:04 AM
Hello @EmdSTM32WL and welcome to the ST Community :smiling_face_with_smiling_eyes:.
Usually, the STM32WL can give a range of a few kilometers for the same configurations that you are using. I suggest you give more details about your HW configurations (the antenna that you are using, any changes that you have done on your HW,...).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-14 6:39 AM
Hi STTwo-32,
Thank you for your quick reply.
I'm using STBoard : STM32-Nucleo 64 WL55JC , two boards , one as Gateway and another as End-device. , below you find.
Using the Antenna equipped alrerady with the board I made just 100metres , so I changed with another Antenna ( below you find the link of the antenna) , and I can increse the range to 300m , but it's not enough
Link Antenna : GSM/GPRS Magnetic Antenna | Mikroe
PS : I'm using Nucleo-WL55JC1 ( high band).
For the SW I'm using the ST demonstartion in SMTE32WL FW.
I'm very blocked with this issue.
Thank you in advance.
Best Regards
2023-11-14 8:05 AM
Hello again @EmdSTM32WL
I suggest you to.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-15 1:21 PM
Hi STTwo-32 ,
I tested as your suggestion , but no results.
with SF=7 , some meters to get communication.
Ps : I'm using Nucleo Board and the ST FW , I don't made any hardware change.
Any Solution please !
Best Regards
2023-11-22 8:02 AM
Hello @EmdSTM32WL
Can you give more details about your project (the gatway that you are using, the envirenement, ...)
Best regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-22 9:27 AM
As the spreading factor increase, the bps drops significantly, watch the timeout.
The old B-L072Z-LRWAN1 board at 20 dBm could get signals 14KM LoS in a point-to-point test with the slowest most conservative settings.
https://www.mouser.com/new/stmicroelectronics/stmicro-stm32-lorawan-discovery-board/
The placement and configuration of the gateway are likely to dramatically impact distance and success.
2024-01-08 6:37 AM - edited 2024-01-08 6:42 AM
Hello ,
I'm using the same type of board as Gateway and End device.
It' is : NUCLEO-WL55JC
One NUCLEO WL55JC as Gateway and others cards NUCLEO WL55JC as end device.
I have problem with range !
Thank you in advance.
Best Regrads,
2024-01-08 6:45 AM
Hello DeLorean,
Thank you for your message.
I made all SW and HW using the NUCLEO-WL55JC.
for this reason i 'm searching a solution around this baord.
by the way , you use the same board as Gateway also ?
Best Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.