2020-02-13 7:01 AM
I have managed to build the STM32WB Zigbee example applications using Atollic TrueStudio after some massaging. When I program the STM32WB Nucleo board with the binaries that I build, however, the program enters a hardfault when it calls into the provided library for zigbee operations with the coprocessor, stm32wb_zigbee_wb_lib.a.
I have also tried building this project using a trial version of IAR embedded workbench, the IDE for which the project is provided. When I load THAT binary, the program is able to execute successfully.
Other notes:
Any guidance on how to approach this issue would be greatly appreciated; has anyone been able to get this program running without purchasing IAR?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.