2020-02-12 10:09 PM
I have a struct defined as:
struct sendIP_struct {
char node_type[12];
char description[8];
uint32_t uid;
} msgSendMyIP = { .node_type = NODE_TYPE, .description = NODE_DESCRIPTION, .uid = 0 };I take this struct and append it to a thread response message by calling otMessageAppend with no resulting errors. However, what I noticed is that if I pass this struct with .uid defined as anything but 0, otCoapSendResponse returns OT_ERROR_PARSE.
Per RFC 7252, section 5.2.1, I am trying to do a legal "piggybacked" response to a GET request.
After further testing, I found that it did work when I changed the last element in the struct from uint32_t to uint64_t.
struct sendIP_struct {
char node_type[12];
char description[8];
uint64_t uid;
} msgSendMyIP = { .node_type = NODE_TYPE, .description = NODE_DESCRIPTION, .uid = 0 };I set .uid to a value other than null and it all seemed to work just fine with the response being sent and no errors returned.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.