2022-08-21 6:53 AM
We are using B-L072Z-LRWAN1 for developing our application. We are struggling to send more than 11 bytes of application payload. As long as the total payload is 11 bytes, the node joins the network with no issues. When we try to change the DR > 0 so we can push payload more than 11 bytes, then we need null data on fort 0 and the DR is reset back to DR 0 on the node after a join acceptance.
How do we properly change the DR to send data of more than 11 bytes? We are using US 915. Any insights from this forum members will be appreciated.
Sincerely,
Sid
2022-08-21 1:48 PM
The payload length obvious depends on the region.Look at some End_Node/LoRaWAN/App/src/main.c file:
AppData.Buff[i++] = humidity & 0xFF; (Byte number 11)
#if defined( REGION_US915 ) || defined ( REGION_AU915 )
/* The maximum payload size does not allow to send more data for lowest DRs */
#else
2022-08-21 9:15 PM
Yes agreed. We tried changing to DR 1 so we can send more than 11 bytes. DR 1 should allow 51 bytes. However, it does not work.
2022-08-21 9:16 PM
Yes agreed. We tried changing to DR 1 so we can send more than 11 bytes. DR 1 should allow 51 bytes. However, it does not work.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.