NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello everyone, I have recently started learning C language and I am kind of new into embedded systems. I am using NUCLEO WB15CC and trying to develop a system using VL53L1X with MPU6050 sensors. I am getting two sensor data successfully every time I...
Hello,I wanted to ask if it would be possible to have the sequence of commands sent and how they should be formatted, by the STM32CubeMonitorRF tool to the board, so possibly I can recreate those steps even with a custom program.Thank you very much
Hello,We have an issue updating the stack programmatically.Following the AN5185 (section 2.1) we put the new stack binary (stm32wb5x_BLE_Stack_full_fw_1.13.1.bin) at 0x0809A000 - 45 sectors before 0x080C7000 (stack start for 1mb model) - trying to u...
Hello. I am using a NUCLEO-WB15CC board trying to build a BLE application.I followed the instruction from a YT video by STM: https://www.youtube.com/watch?v=i10X4Blr8nsI generated code with CubeMX version6-5-0 on linux.The code called HardFaultHandle...
Hello! The title pretty much says it all - I'm trying to figure out how to configure BLE between two B-U585I-IOT02A boards, but establishing the BLE connection is a bit confusing to me. Am I able to configure it from the UFBGA169 IOC file in STM32Cub...
I have setup USB connectivity between the STM32WB55 Nucleo board and my pc.As I connect to the board, my application sends some data and the board response accordingly. I can send another command to start the application running on the hardware, whic...
Hello.I'm planning a project that will use large amount of flash memory, therefore, I will need to be cautious with memory saved for app updates. I'm using STM32WB55VGQ6 with 1MB of flash memory on custom designed board. my current application is abo...
Hi there,I am using an STM32WLE with an input voltage range of 2 - 3.3V. It will eventually be powered by a lithium coin cell, but I am currently using a benchtop power supply. The datasheet states that both the MCU and the radio should function down...
Working on project with BLE interface and need to add I2C interface to read a sensor. Started with BLE Heartrate example (it wakes up ever 1s which I also need to do) and added I2C by using CubeMX to generate the new code. To start testing I added th...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.