2023-04-25 11:14 PM - last edited on 2025-06-04 8:21 AM by Andrew Neil
why icubelrwan stack does not support stm32f407.
How I can use stm32nucleol476rg as lora end node using icubelrwan stack.
Solved! Go to Solution.
2023-04-25 11:42 PM
Ah, I forgot to answer the second question: you can find a few projects with the NUCLEO-L476RG in the firmware archive at the above URL under
Projects\NUCLEO-L476RG\Applications
Good luck!
/Peter
2023-04-25 11:40 PM
Welcome, @Mshin.2, to the community!
LoRa is a transmission method that can bridge large distances with extremely little energy. Ultra-low-power devices were specially developed for this purpose, so that they can work for a long time with a small battery or other weak energy source, for example.
The STM32L series was the first to fulfil this ultra-low power approach. An STM32F407, although very powerful, is a power waster compared to the ultra-low-power STM32L devices, which is the reason why only STM32L are currently supported by I-CUBE-LRWAN.
Nevertheless, it would be possible to port the stack to another platform, which you can certainly do yourself with the source code provided, can't you?
Regards
/Peter
2023-04-25 11:42 PM
Ah, I forgot to answer the second question: you can find a few projects with the NUCLEO-L476RG in the firmware archive at the above URL under
Projects\NUCLEO-L476RG\Applications
Good luck!
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.