2020-10-15 1:48 AM
I got some STM32WB55CG samples from st office and the date code is 034. The read out FUS version is 1.1.0. Has the default firmware been upgraded? So the customer doesn't have to upgrade FUS anymore?
D:\Program Files\STMicroelectronics\stm32cube\STM32CubeProgrammer\bin>STM32_Programmer_CLI.exe -c port=SWD mode=HOTPLUG -r32 0x20030030 4 -r32 0x20030024 50
-------------------------------------------------------------------
STM32CubeProgrammer v2.5.0
-------------------------------------------------------------------
ST-LINK SN : 32FF6C063047463341421351
ST-LINK FW : V2J37S7
Board : --
Voltage : 3.23V
SWD freq : 4000 KHz
Connect mode: Hot Plug
Reset mode : Software reset
Device ID : 0x495
Revision ID : Rev Y
Device name : STM32WBxx
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M0+/M4
Reading 32-bit memory content
Size : 4 Bytes
Address: : 0x20030030
0x20030030 : 01010100
Reading 32-bit memory content
Size : 52 Bytes
Address: : 0x20030024
0x20030024 : A94656B9 00000001 01010000 01010100
0x20030034 : 00000006 00000000 00000000 00000000
0x20030044 : 00000000 00000000 00658473 0080E126
0x20030054 : 00000496
Solved! Go to Solution.
2020-10-16 5:56 AM
Hi,
I have an STM32WB55 Nucleo Pack. The FUS version was 053 (I don't remember the correct number, but it is old version) which needed upgrade. So I deleted the current version and now I am stuck.Not able to upgrade to newer version as I keep getting wrong address message, though I followed the addresses given in the table for binaries. Hope I don't have to kiss goodbye to this board set. Please help. Thank you.
2020-10-16 6:08 AM
Note that you never can delete the FUS as it located in a protected area. Use the USB port in DFU mode to read the FUS version at 0x20030030.
Please download all the option bytes to understand the status of your board.
2020-10-16 9:43 AM
Hello Remi QUINTIN,
Thank you very much for your suggestion. I will check version as suggested and post. How do I download all option bytes? I will check how to read them but will be obliged if you can provide a link to all the commands. Regards
2020-10-16 9:50 AM
To display the option byte you can use CubeProgrammer in CLI mode. In that case the command is
STM32_Programmer_CLI.exe -c port=usb1 -ob displ
Or you can use CubeProgrammer in GUI mode.
In that just make a screen shot of the Option Bytes section (OB).
2020-10-16 9:53 AM
Hi Remi QUINTIN,
Thank you so much for immediate reply. Helps a lot. Will post the bits so you can guide further.
Best Regards
NPS
2020-10-16 10:06 AM
2020-10-16 10:07 AM
2020-10-16 10:08 AM
2020-10-16 10:09 AM
2020-10-16 10:26 AM
OK. So according to the SFSA value (0xF6), your FUS version is still V0.5.3 which is the very first version of FUS.
You have to upgrade it to be able to program one of the RF stack of the latest CubeWB FW pacakage.
Please use the last CubeWB FW package v1.9.
Perform a mass erase of the flash memory. Dont worry , you will get an error when the tool tries to erase the FUS protected sectors (above SFSA location). But in the end, the user part of the memory becomes clean.
Then perform a fwdelete. Here you may not need it as there is no RF stack on your chip curently.
Then program the stm32wb5x_FUS_fw_1_0_2.bin binary (= FUS V1.0.2)
Then program the stm32wb5x_FUS_fw..bin binary (= FUS V1.1.0)
Then program the RF stack you want using the start address listed in the release notes.
Finnaly program your application at 0x08000000.
Normally it should work!!! anyhow cross the fingers, it may help :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.