STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

When the data of IEEE802.15.4 is transmitted by STM32WB55, ACK is returned from the communication partner, but STM32WB55 does not recognize ACK.

HelloWe are currently using sample Mac_802_15_4_FFD to verify IEEE 802.15.4 transmission on the STM32WB55 Nucleo Pack board. The protocol stack is stm32wb5x_Mac_802_15_4_fw.bin V1.90.I have sent data (MAC_MCPSDataReq) that requires ACK (ack_Tx = 0x01...

MNitt.1 by Associate II
  • 938 Views
  • 0 replies
  • 0 kudos

Resolved! Advertise don't run in HearthRateFreeRTOS project

Hello!I have created a new project based on the ST example BLE_HeartRateFreeRTOS. I made the comparisons between both projects and added what was missing in my project. I think that I have copied everything that I should but the advertising doesn't s...

Kolab by Senior
  • 3223 Views
  • 10 replies
  • 0 kudos

TIM2 PWM is not working on P-Nucleo-wb55

I have set the TIM2 with the following code: __HAL_RCC_TIM2_CLK_ENABLE();   htim2.Instance = TIM2; htim2.Init.Prescaler = 0; htim2.Init.Period = 80; htim2.Init.RepetitionCounter = 0; htim2.Init.ClockDivision = TIM_CL...

MSamy.1 by Associate II
  • 2364 Views
  • 4 replies
  • 0 kudos

How can our app connect to STM32WB55 without using STM apps?

For our senior design project, we're trying to pair our created phone app (android) with the STM32WB55. Unfortunately, the WB55 only bluetooth pairs with apps created by STMicroelectronics. How do we use our app to connect to the WB55 without having ...

NVeda.2 by Associate
  • 1349 Views
  • 1 replies
  • 0 kudos

Hello, I have a STM32L073 Nucleo board and SX1261 Lora Radio Board. I am using STM Cube LoRaWAN package to develop a Class A End Node. I want to use GPIO External Interrupt, Any suggestions how to implement?

msp.c has a callback definitionvoid HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) { HW_GPIO_IrqHandler(GPIO_Pin); }it.c has the followingvoid EXTI4_15_IRQHandler(void) { HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_4); HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_5); ...

BSada.1 by Associate
  • 1675 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.