2018-01-19 8:25 AM
Hello.
I was working with the LRWAN software using the Murata module a couple of months ago and was happy with its operation and functionality on my custom PCB. I moved over to hardware/antenna development and now have a board whose performance I am happy with.
However I have now moved back into software development and noticed that the LRWAN software had moved up a few revisions. I was working with 1.1.1 and so I downloaded the latest (1.1.4), configured everything and now find that although I can successfully perform an uplink and downlink, I am not receiving a confirmation when I turn on confirmed messages (using AT+CFM=1). When I load up my previous project (1.1.1) confirmed messages work fine.
I'm trying to pin down why this is and am trying to download a fresh copy of 1.1.1. as well as 1.1.2 and 1.1.3 so that I can track the changes which may have resulted this problem. However, I cannot locate the archive of previous versions.
Has anyone else run into the confirmed messages issue, or can anyone point me to an archive?
I'm using the ABZ module on a custom board.
Gateway is a Multitech Conduit.
Using the Keil uVision 5.23 IDE
Using the project located in STM32CubeExpansion_LRWAN_V1.1.4\Projects\Multi\Applications\LoRa\AT_Slave\MDK-ARM\B-L072Z-LRWAN1
Many thanks,
Ben.
#lora #i-cube-lrwan #abz #confirmed-messages2018-07-02 9:24 AM
https://drive.google.com/open?id=1WVC5AQf_Vv3XjY-qReTYlxqkaWbkC0qD
https://drive.google.com/open?id=1s6FfDQi7rhOwWhw1iOlF76DH0ag9gM3v
https://drive.google.com/open?id=1SYHOx9jT-9aGuezWvDsqtuSpUr-06Bhk
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.