2018-01-19 8:25 AM
Hello.
I was working with the LRWAN software using the Murata module a couple of months ago and was happy with its operation and functionality on my custom PCB. I moved over to hardware/antenna development and now have a board whose performance I am happy with.
However I have now moved back into software development and noticed that the LRWAN software had moved up a few revisions. I was working with 1.1.1 and so I downloaded the latest (1.1.4), configured everything and now find that although I can successfully perform an uplink and downlink, I am not receiving a confirmation when I turn on confirmed messages (using AT+CFM=1). When I load up my previous project (1.1.1) confirmed messages work fine.
I'm trying to pin down why this is and am trying to download a fresh copy of 1.1.1. as well as 1.1.2 and 1.1.3 so that I can track the changes which may have resulted this problem. However, I cannot locate the archive of previous versions.
Has anyone else run into the confirmed messages issue, or can anyone point me to an archive?
I'm using the ABZ module on a custom board.
Gateway is a Multitech Conduit.
Using the Keil uVision 5.23 IDE
Using the project located in STM32CubeExpansion_LRWAN_V1.1.4\Projects\Multi\Applications\LoRa\AT_Slave\MDK-ARM\B-L072Z-LRWAN1
Many thanks,
Ben.
#lora #i-cube-lrwan #abz #confirmed-messages2018-01-19 10:06 AM
Hello.
Been working some more on this and I believe I've discovered the root cause.
It appears as though the ABZ module is actually receiving the confirmation OK, however, the AT+CFS=? was returning the wrong answer.
Compared to version 1.1.1, there has been a line removed from Lora.c which would appear to be essential to getting a correct answer. I'm not sure where this change originated as I do not have access to 1.1.2 or 1.1.3.
Within McpsConfirm() the first line in 1.1.1 assigned the confirmation data stored in mcpsConfirm to lora_config.McpsConfirm. It is
lora_config.McpsConfirm that is checked when AT+CFS is queried, however, it remains null as it was never assigned to.
Adding the following line back into McpsConfirm() returns expected functionality:
lora_config.McpsConfirm = mcpsConfirm;
My concern is that this line was removed for a reason, so maybe this is not the correct way to return functionality? Perhaps instead mcpsConfirm was meant to be checked in lora_config_isack_get() and this change was forgotten?
Feedback would be very gratefully received!
Ben.
2018-01-19 12:05 PM
I don't have 1.1.3, didn't see that being available
Here is my mirror of 1.1.2
https://drive.google.com/open?id=0B7OY5pub_GfIckZ5Sjd5Z3M5c00
2018-01-19 2:40 PM
,
,
No, I didn't see 1.1.3, either - just have 1.1.2 and 1.1.4
EDIT
There appears to be an archive of 1.1.1 - 1.1.4 here: ,
https://www.stmcu.jp/design/sw_dev/firmware/54690/ ♯ 546900_en
, ,- Japanese site.My normal login doesn't seem to work there - I guess you would have to re-register there ?
2018-01-19 2:48 PM
My post with link is stuck in moderation. It says:
No, I didn't see 1.1.3, either - just have 1.1.2 and 1.1.4
There appears to be an archive of 1.1.1 - 1.1.4 on the ST Japanese site. My normal login doesn't seem to work there - I guess
you would have to re-register there ?
2018-01-19 5:27 PM
https://drive.google.com/open?id=0B7OY5pub_GfIYmZtQXhaRzNHbkk
https://drive.google.com/open?id=0B7OY5pub_GfIdk1iNlU3MzZQOVk
https://drive.google.com/open?id=0B7OY5pub_GfIckZ5Sjd5Z3M5c00
2018-01-20 4:27 PM
Requested a copy of v1.1.3 from my local FAE
2018-01-20 5:50 PM
Never mind, I registered
https://drive.google.com/open?id=1WVC5AQf_Vv3XjY-qReTYlxqkaWbkC0qD
2018-01-22 4:39 AM
Thank you so much for linking the previous versions. So it appears as though the line disappears in v1.1.3. Have you had issues with confirmed messages in v1.1.4?
2018-01-22 6:17 AM
Haven't actually tried it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.