STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! Mesh network with NUCLEO-WL55JC

Hello,I am currently working on a collar localization project using NUCLEO-WL55JC cards. My job is to create a mesh network using these boards. We have: 1 card which acts as a Gateway (connected to an application), 1 card which is used to simulate th...

KYZ by Associate III
  • 1157 Views
  • 2 replies
  • 0 kudos

Resolved! Cannot run any example on Nucleo-WB55RG board

I cannot run any example on p-nucleo-stm32wb55 board.i only receive this message on debug. Wireless Firmware version 1.22.1Wireless Firmware build 1FUS version 2.0.0>>== SHCI_SUB_EVT_CODE_READY>>== SHCI_SUB_EVT_CODE_READY - FUS_FW_RUNNING I updated F...

Resolved! STM32WL33 data coding

I'm transmitting a custom packet by the NUCLEO-WL33CC2 and I'm receiving the pachet by a different harware that use the SI4460 tranceiver from Silabs. In the receiver board I receive the pachet, but the byte are completely differents than the byte I ...

sbelcatronic_0-1748004288054.png

CubeMX setting incorrect baudrate for STM32WL33CC LPUART

Hi All,1. [Part Number] STM32WL33CC12. [Environment] Windows OS, STM32CubeIDE version 1.17.0, Firmware package STM32Cube FW_WL3 V1.0.03. [Schematics] STM32 Nucleo-64 development board4. [Details] See below.5. [Expected behavior] Data sent at 115200 f...

ola by Associate III
  • 2822 Views
  • 5 replies
  • 2 kudos

Resolved! STM32WLE5 Max allowed power on RFO_HP pin

Hi ,when the SUBGHZ block is in TX mode. if , for example , the COAX cable connected to the board SMA connector is suddenly disconnected during RF TX transmission .what is the maximum allowed input power on the RFO_HP pin when operating in TX mode ? ...

viola by Associate III
  • 1225 Views
  • 2 replies
  • 0 kudos

ACI_HAL_FW_ERROR_VSEVT_CODE error 0x02

Hi all After connecting to my STM32WBA i get the following program trace:>>== HCI_LE_CONNECTION_COMPLETE_SUBEVT_CODE - Connection handle: 0x0001- Connection established with @:5c:c7:a3:61:de:70- Connection Interval: 30.00 ms- Connection latency: 0- S...

cvs_dev by Associate II
  • 775 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.