STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! bt_enable() fails with Zephyr/nucleo-WB55RG

I try to initialize bt, with bt_enable() in zephyr. So far, no success,it returns me a -19 error ( not found )Any help would be very appreciated.Note: I am using Zephyr ( not Cube/HAL ).Context:- Zephyr 4.1.99- Board stm32 nucleo-wb55rg- FUS version ...

Resolved! Unclean I2C - STM32WL5MOCH

The I2C on our board is unclean, at all clock speeds - 1 MHz, 400 kHz and 100 kHz - even without rf circuitry running.  Signal traces are about 5 cm long in total.  Pullups were set at 1 kOhm to enable Fast Mode Plus, but even the Standard 100 kHz lo...

Captures1.PNG Captures2.PNG Captures.PNG Capture.PNG

Resolved! How to use uart at wb55 BLE Mode

当 wb55 启用 BLE 并同时使用 UART1 的 CFG_HW-UART1 时,如何再次使用 UART 进行串口传输? 不使用 APP_SBG_SG 等函数,而是使用 HAL 等函数UART_Transmit

Thorn by Associate
  • 978 Views
  • 1 replies
  • 0 kudos

stm32wba52cg Antenna design on PCB

Hello, I hope this message finds you well. We are currently working with the STM32WBA52CG MCU and have designed an antenna based on the development board specifications. I would like to seek your advice regarding the placement of the antenna as shown...

Hitesh2022_0-1748522971742.png

STM32WLE: what is RTC mixed mode good for?

Setting RTC binary mixed mode on STM32WLE leads to normal operation of BCD Alarm and wake-up counter plus their wakeup and IRQ triggering-so far so good. It behaves similar when set to binary mode only - binary alarm etc work as expected. So what is ...

PBE by Associate
  • 1047 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.