STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! LE Audio QoS Configuration Failed in STM32WBA55G-DK1

When I checked the LE Audio unicast operation of the provided project on the STM32WBA55G-DK1, I noticed a strange behavior.For the peripheral, the PAC settings are Sink 2, Src 1, but when I perform QoS Configuration using the following procedure, the...

Jetson by Associate II
  • 3212 Views
  • 7 replies
  • 3 kudos

Using an NFC Antenna with the STM32WBMMG

I am wanting to add the STM32WBMMG to my board but it will need to be compatible with an external NFC antenna so I can have cellular communication. Is this possible and how would I go about implementing this?If it is not possible are there other STM ...

Hbburnha by Associate II
  • 815 Views
  • 1 replies
  • 0 kudos

STM32WB05xN changing hardware configurations

I am planning to use the STM32WB05KN as a network coprocessor for a STM32U0. The Nucleo board has both LSE and HSE populated, but since my PCB is space constrained, I would like to use the internal oscillators instead of external and also turn off SM...

Screenshot 2025-05-07 at 5.15.36 PM.png image.png

Resolved! No Button interrupt PA0 in SubGHz sequencer code

Hi all, So to my surprise, I have issues getting a button press to work in a Lora PingPong sequencer example, and I can't find any relevant posts, so ...The part I'm using WLE5.The ping-pong code is working fine, but I wanted to add a button to start...

Micael by Associate II
  • 1016 Views
  • 1 replies
  • 0 kudos

Resolved! NUCLEO-wl55jc StandBy mode

Hello everyone !I'm currently working on the STM NUCLEO-wl55jc card and I'm having a few problems with it.I'm using the Ping Pong example code, which allows LoRa point-to-point communication between 2 cards. This works perfectly.My problem now is tha...

KYZ by Associate III
  • 1671 Views
  • 4 replies
  • 0 kudos

Resolved! STM32WB05KZ Flashing Issue

Hello everyone,I have encountered an issue with the STM32WB05KZ on a custom board which only allows me to flash the board under very specific conditions. The first time out of the box, everything works fine, I can flash using a ST-LINK V3-PWR straigh...

JSGraaf by Associate III
  • 2019 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.