STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

STM32WLE5CCU6 LoRa Antenna design review

Hi,I want to design my own LoRa-Board based on an STM32WLE-Chip. It is my first time handling with RF-related topics which is why I'm creating this post. I created a design which I would want to have reviewed for major flaws, so I can order my first ...

Resolved! Programmed STM32WLE5CC

Greetings,To start with stm32 wireless series i bought STM32WLE5CC and uploaded my custom code of gpio toggeling without initialiazing PA13 and PA14 for serial wire debug. The program runs as it should but when i try to re-flash the controller with S...

B-WB1M-WPAN1

Colleagues,I need to implement the BLE_CableReplacement project on the b_wb1m_wpan1 device. Since I don’t know the services of this project (the BLE_CableReplacement.ioc file is not included), I tried to adapt the project for the b_wb1m_wpan1 device ...

STM32WBDK LPM wont allow PWM to work

 I’m driving a hobby servo on the STM32WB5MM-DK Discovery board using TIM2 PWM and the STM32CubeWB Sequencer/LPM utilities. When I disable low-power mode entirely, the servo moves flawlessly on each 500 ms button-hold toggle. But as soon as I allow t...

Resolved! Nucleo-wl55jc - LDO / SMPS

Hello everyone,I'm using Nucleo-wl55JC boards with the PingPong example code (which is working). I saw in the datasheet that we could have 2 different power supplies LDO and SMPS, I also saw that the SMPS mode was more economical than LDO, that's why...

KYZ by Associate III
  • 1172 Views
  • 2 replies
  • 0 kudos

STM32WL reset in debugger mode

Hello All,I am working on STM32WLE5 , and low power mode used for controller is stop 2 mode. And I am using MSI at 4Mhz  as system clock. When i enable debugger mode, controller takes reset after a while and reset type shown is also not correct. Whil...

Ronik_123 by Associate II
  • 1048 Views
  • 4 replies
  • 0 kudos

Resolved! STM32WB55 Error on start of BLE stack

Hi,I'm currently trying to get Bluetooth working from Zephyr. I'm working with the Zephyr sample codezephyr\samples\bluetooth\peripheral_dis.I'm using a Nucleo-WB55RG board. Using STMCubeProgrammer I've loaded the FUS at 0x080EE000 and the file stm32...

Lee_T by Associate II
  • 3477 Views
  • 11 replies
  • 1 kudos

I-CUBE-LRWAN support for STM32U5 + SX1262

I was wondering if anyone had managed to get the LoRaWAN End-Node example running on other MCUs than the STM32L series. I've been trying to get it to run on the STM32U5A9 combined with an SX1262, but I haven't had any luck. I'm trying to integrate th...

JSGraaf by Associate III
  • 1332 Views
  • 2 replies
  • 0 kudos

difference between MCUs firmware

Hello,      I would like to know if fw developed in stm32cubeIDE for nucleo wl55jc1(there are some examples for it) is compatible with https://www.st.com/en/microcontrollers-microprocessors/stm32wle5cc.html mcu family(stm32wle5ccu6) or I should expec...

Matching networks

HiIm a bit new and have som RF related question.I am doing a heart monitoring project where i want to measure ECG signals, put it through my AFE (analog frontend), then into the ADC inside the MCU and then output the data through BLE into a phone. I ...

siyar by Associate II
  • 869 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.