2025-06-24 9:06 PM
I’m driving a hobby servo on the STM32WB5MM-DK Discovery board using TIM2 PWM and the STM32CubeWB Sequencer/LPM utilities. When I disable low-power mode entirely, the servo moves flawlessly on each 500 ms button-hold toggle. But as soon as I allow the LPM manager to enter Stop mode, the PWM pulses become unstable and the servo either jitters or stops moving.
PWM in Stop Mode: Are there proven techniques to retain stable PWM outputs during Stop or Low-Power Run modes on STM32WB series?
Sequencer Integration: Can anyone share examples of driving servos reliably while staying in LPM using the Utility Sequencer?
I have uploaded the project.
2025-06-24 11:24 PM
Hello,
if you want to generate a PWM signal in LP mode, you could use a LP timer.
Please kindly read section 27 in RM.
If you have any other question, please let me know.
Best regards,
Filip Kremen
2025-06-25 12:14 AM
I was expecting to have better control over the application as in not enter low power mode before the button event is set. Could you please have a look at my application code and suggest me a way to do so.
2025-06-25 5:16 AM
Hello,
I have quickly checked your project, can you please try to move UTIL_LPM_SetStopMode(1U << CFG_LPM_APP, UTIL_LPM_ENABLE) function at the end of PWM_timer_ISR()? This will enable stop mode after stopping the PWM signal.
Best regards,
Filip Kremen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.