STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

STM32WL33xx: How to increase the wakeup radio distance?

What settings can be changed in LPAWUR_WakeupRadio_Rx code to increase the wakeup radio distance?From data sheet ,  The STM32WL33xx RF output power can be programmed to deliver up to +20 dBm, in TX+TXHP mode, and in MRSUBG_WakeupRadio_Tx code,MRSUBG_...

Gwo by Associate II
  • 940 Views
  • 1 replies
  • 0 kudos

Resolved! NUCLEO-WB55RG board FW update

Hello, I have recently started getting familiarized with the P-NUCLEO-WB55 kit, and I have run to my first big mess up. I was attempting to perform a wireless stack FUS routine over the STLink interface, and I might have set a wrong start address for...

Problem with RTC Alarm, LSE, or power up?

Hi,I'm having a problem with the LSE/RTC and I'm not exactly sure where to start, but I'll try to explain it.I'm using the STM32WB55 and the RTC is used for FreeRTOS tick timing. It works perfectly during normal operation with a 1 ms tick, and it als...

JR2963 by Senior II
  • 1012 Views
  • 4 replies
  • 0 kudos

Resolved! Why STM32WB15CC as a GATT server is not detected in ST BLE Toolbox after following "STM32WB Getting Started : Part 12b, Lab. Receiving data from the phone" video

Hi, I try to create a GATT server with a NUCLEO-WB15CC.I'm a beginner with STM32WB MCUs so I followed the Getting Started Series video and particulary : "STM32WB Getting Started Series: Part 12b, Lab. Receiving data from the phone" When its came time...

Resolved! Zigbee reconnect problem

I'm trying to develop an application for zigbee for the stm32wb55, but i get some problems when I try to reconnect.The configuration for the coordinator its the next parameters:      - config.startupControl = ZbStartTypeForm;      - config.extendedPa...

Pablo1610 by Associate II
  • 9287 Views
  • 7 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.