2018-05-04 4:54 AM
Hi,
if I build the programm 'AT-Slave' (STMCubeExpansion_LRWAN) I got an License Error from Keil ( error: L6050U: The code size of this image (38072 bytes) exceeds the maximum allowed for this version of the linker.). It is possible to reduce the code size from the example without losing the function?
#at_slave #keil-mdk5 #b-l072z-lrwan12018-05-04 5:35 AM
Use the free licence
http://www2.keil.com/stmicroelectronics-stm32/mdk
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.