2018-05-28 1:41 PM
Hi! I'm looking for some help in getting my STM32L476RG and IDW01M1 up and running with the FP-CLD-AZURE1 STM32Cube function pack. I also have the sensors.
I've flashed the board with the relevant binaries etc... The Azure_Sns_DM program accepts my azure and WiFi variables but just seems to hang after getting to the connection string:
Output below:
UART Initialized
I2C InitializedSTMicroelectronics Azure_Sns_DM:
Version 3.3.0 STM32L476RG-Nucleo board Azure SDK Version 1.1.31Ok Accelero SensorOk Gyroscope SensorOk Magneto SensorOk Humidity SensorOk Temperature Sensor1Ok Temperature Sensor2Ok Pressure SensorEnabled Accelero SensorEnabled Gyroscope SensorEnabled Magneto SensorEnabled Humidity SensorEnabled Temperature Sensor1Enabled Temperature Sensor2Enabled Pressure Sensor (HAL 1.8.2_0) Compiled May 26 2018 08:21:23 (openstm32) OTA with one HTTP HEAD + Multiple HTTP one GET of 1024BytesTesting BootLoaderCompliance: Version 1.2.0 BL Version Ok MagicNum Ok MaxSize 0x7c000 OTAStartAdd OkBootLoader Compliant with FOTA procedureInit Application's TimersInit Random Number GeneratorEnabled Free FallInit WIFI's TimersInit WIFI's UART1--------------------------| WIFI Credential |--------------------------Meta Data Manager read from FlashMeta Data Manager version=0.8.0 Generic Meta Data found: WIFI Size=81 [bytes] AZURE Size=256 [bytes] Default SSID : <redacted> Default PassWd : <redacted> Default EncMode: WPA2/WPA2-PersonalWait 3 seconds for allowing User Button Control for changing it--------------------------| Connection String |-------------------------- Default Connection String : <redacted>Wait 3 seconds for allowing User Button Control for changing itI can't for the life of me see whats going on after this point - AT commands don't seem to work.
If I could get some debug from the terminal that might give me a clue - but as I'm a newbie at all this I'm struggling...
Any help appreciated!
Thanks
Darren#stm32-wifi #idw01m1We’re moving the ST Community to a new platform to give you a better and more reliable community experience.