2018-06-05 12:24 AM
Hi everyone,
I'm working on B-L072Z-LRWAN1 lora discovery kit and i have an issue.
I'm able to upload my program on STM32 and it run when the STM is plug in on USB STLINK.
My issue is when i want run my STM on 3AAA battery.
I just have the LD7 LED and my program (send data with LoRa) seems to not working ...
Have you an idea ?
Thanks
PS : i use the EndNode Cube default project
#battery #lora2018-07-10 7:26 AM
Same problem here, using SW4STM32 and latest ST-Link firmware (I thought it could help as indicated in
https://os.mbed.com/questions/68969/STM32F429I-DISC1-can-not-be-powered-by-u/
). Seems like MCU is blocked without USB host connection.Thx for any advice.
2018-07-10 7:41 AM
Ok, the problem is RESET pin as mentioned in UM2115: 'If the board is supplied by CN13, by battery or by CN11, SB37 must be removed to release the RESET pin managed by ST-LINK. In that case the ST-LINK is no more powered.'
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.